adccommunitymod (AutomationDirect) asked a question.

D2-250 and F2-08AD2

Created Date: December 12,2000

Created By: grignon

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am attempting to set up the pointer method of extracting data from an F2-08AD2 in slot 3 into Vmemory, as per page 5-11 of the A-D manual: However, when I specify V7663 as the destination for the Data type/# of Channels constant, the Directsoft 32 program returns an "Invalid Element " error. The 250 CPU version is 1.46, which the manual says should support this setup.


  • adccommunitymod (AutomationDirect)

    Created Date: December 12,2000

    Created by: grignon

    I am attempting to set up the pointer method of extracting data from an F2-08AD2 in slot 3 into Vmemory, as per page 5-11 of the A-D manual:

    However, when I specify V7663 as the destination for the Data type/# of Channels constant, the Directsoft 32 program returns an "Invalid Element " error.

    The 250 CPU version is 1.46, which the manual says should support this setup.

    Expand Post