adccommunitymod (AutomationDirect) asked a question.

NTP through the StrideLink VPN device

Created Date: June 11,2019

Created By: Ryan_Poethke

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have a BRX PLC behind a StrideLink VPN device. Once per week, I would like the PLC to enable the VPN device (allow outside connection) and use the NETTIME instruction to retrieve the current time and date from the NTP server at 0.pool.ntp.org I 've got the logic in the PLC set to enable the VPN device every Sunday morning between 2:00:00 and 2:00:59. At 2:00:00 + (20) seconds, the PLC triggers the NETTIME instruction. What, if anything, do I need to do with the StrideLink VPN device to allow this to work? Does StrideLink have a NPT server I can use, or will any NTP server work? Thanks, Ryan Poethke


  • adccommunitymod (AutomationDirect)

    Created Date: June 11,2019

    Created by: Ryan_Poethke

    I have a BRX PLC behind a StrideLink VPN device. Once per week, I would like the PLC to enable the VPN device (allow outside connection) and use the NETTIME instruction to retrieve the current time and date from the NTP server at 0.pool.ntp.org I 've got the logic in the PLC set to enable the VPN device every Sunday morning between 2:00:00 and 2:00:59. At 2:00:00 + (20) seconds, the PLC triggers the NETTIME instruction.

    What, if anything, do I need to do with the StrideLink VPN device to allow this to work? Does StrideLink have a NPT server I can use, or will any NTP server work?

    Thanks,

    Ryan Poethke

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 11,2019

    Created by: BobO

    Don't know if it is relevant to your effort, but Do-more uses SNTP, not NTP. Don't remember what the major differences are, but ports should be different.

  • adccommunitymod (AutomationDirect)

    Created Date: June 12,2019

    Created by: Ryan_Poethke

    Don't know if it is relevant to your effort, but Do-more uses SNTP, not NTP. Don't remember what the major differences are, but ports should be different.

    Does this mean that the following quote from the Help file for NETTIME is incorrect?

    "This instruction can use either an NTP Server or an SNTP Server as the time server. "

    Thanks,

    Ryan Poethke

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: June 12,2019

    Created by: BobO

    Does this mean that the following quote from the Help file for NETTIME is incorrect?

    "This instruction can use either an NTP Server or an SNTP Server as the time server. "

    Thanks,

    Ryan Poethke

    No, it's right. NTP servers also support SNTP.

    I thought the ports were different, but I misremembered. Been doing this too long...everything blurs together. Disregard.

    Expand Post