adccommunitymod (AutomationDirect) asked a question.

Connectivity issue

Created Date: November 21,2016

Created By: Ajb86

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

We have DL260 plc connected to a EA9T10CL panel. The two are connect with unmanaged switch along with a wifi access piont. About 15 meter away from the plc we have a pc setup where we remote view the hmi over IE. We have an android based tablet with the cmore app that is mounted in the cab of a front end load. When we are running all of this the remote view and the tablet keep dropping out. Today i closed the remote view and kept the tablet on and run everything locally at the hmi and all worked fine. The issue seems to be the remote view and the app running together. Anyone run similar setup and having issues?


  • adccommunitymod (AutomationDirect)

    Created Date: November 21,2016

    Created by: Ajb86

    We have DL260 plc connected to a EA9T10CL panel. The two are connect with unmanaged switch along with a wifi access piont.

    About 15 meter away from the plc we have a pc setup where we remote view the hmi over IE.

    We have an android based tablet with the cmore app that is mounted in the cab of a front end load.

    When we are running all of this the remote view and the tablet keep dropping out.

    Today i closed the remote view and kept the tablet on and run everything locally at the hmi and all worked fine.

    The issue seems to be the remote view and the app running together.

    Anyone run similar setup and having issues?

    Expand Post