adccommunitymod (AutomationDirect) asked a question.

Interfacing DMX Controller to SCADA using modbus RTU

Created Date: March 05,2014

Created By: arclivin

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I want to interface DMX controller with SCADA using Modbus RTU.I am planning to use C0-01DD1-D CLICK PLC as an interface between DMX Controller and SCADA.The DMX controller accepts and responds to simple ASCII commands.The serial port commands that the controller accepts are given as attachment.The response for i00 status command in hyper terminal is also given in the attachment. Please give a technical advice whether the above said PLC model can be used for achieving this if so how to send and receive ASCII commands and reply. Thank you :confused:


  • adccommunitymod (AutomationDirect)

    Created Date: April 27,2014

    Created by: jesshymanc

    Have you solved this already?

  • adccommunitymod (AutomationDirect)

    Created Date: May 02,2014

    Created by: plcnut

    DoMore can do it. There is a thread on here somewhere with some lighting controller samples.

  • adccommunitymod (AutomationDirect)

    Created Date: March 05,2014

    Created by: arclivin

    I want to interface DMX controller with SCADA using Modbus RTU.I am planning to use C0-01DD1-D CLICK PLC as an interface between DMX Controller and SCADA.The DMX controller accepts and responds to simple ASCII commands.The serial port commands that the controller accepts are given as attachment.The response for i00 status command in hyper terminal is also given in the attachment.

    Please give a technical advice whether the above said PLC model can be used for achieving this if so how to send and receive ASCII commands and reply.

    Thank you

    :confused:

    Expand Post