adccommunitymod (AutomationDirect) asked a question.

Lookout state file gets zeroed out occassionally.

Created Date: February 16,2007

Created By: CHARLIE ARNET

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have an application using Lookout (not Lookout Direct) and a driver (the one called DirectLogic) from the DL Plus driver object set. The Lookout application is communicating to a dl260 on a local area ethernet network via the DirectLogic driver object. It works fine, but every once in a while (once or twice a month) all the setpoints in the Lookout application are set to zero inexplicably. I am thinking that something is messing with the state file (ie the file with the .l4t extention) Any ideas or thoughts on this problem?


  • adccommunitymod (AutomationDirect)

    Created Date: February 16,2007

    Created by: CHARLIE ARNET

    I have an application using Lookout (not Lookout Direct) and a driver (the one called DirectLogic) from the DL Plus driver object set. The Lookout application is communicating to a dl260 on a local area ethernet network via the DirectLogic driver object.

    It works fine, but every once in a while (once or twice a month) all the setpoints in the Lookout application are set to zero inexplicably. I am thinking that something is messing with the state file (ie the file with the .l4t extention)

    Any ideas or thoughts on this problem?

    Expand Post