adccommunitymod (AutomationDirect) asked a question.
Created Date: March 14,2006
Created By: squills
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
hello, iam new to these PLCS, My question was is there anyway to sent the port 2 back to the default.. my problem is at first i could connect with no problems, i went to plc mode and changed acouple things. trying to make the plc work for modbus. well for some reason i changed the address to 5 i belive but not sure. now i get the can not connect to plc. I have tried a lot the connection says disabled in yellow.. anyone help??? its a DL06
Created Date: March 14,2006
Created by: Tech Guy
The easy way would be to get a communication cable for port 1. This port is always fixed at 9600 baud and odd parity.
Created Date: March 15,2006
Created by: squills
ok i tryed to connect to com port 1 with the phone line. i connected one side to my laptop and the other to port 1 when i connect it dials my number. should it be dialing a different number. i still can not connect with the erreor trying to connect to unlocked device.also if by chance i did change the address which i dont think i did. Woudl i still be able to connect to comport 1 with address 1?
thanks for help..
Created Date: March 15,2006
Created by: jackson
Port 1 of the PLC is NOT for a modem connection. It is a serial port. Connecting this port to your modem will not work. You need to purchase the D2-DSCBL cable from Automationdirect to connect from the 9 pin serial port of your laptop to the RJ12 port of the PLC.
It is possible that you have damaged the port of the PLC with this connection.
Created Date: March 15,2006
Created by: marksji
Or make your own cable by following the wiring diagram in the manual.
Created Date: May 03,2006
Created by: ThermoT
Are you using Directsoft?
Created Date: March 14,2006
Created by: squills
hello, iam new to these PLCS, My question was is there anyway to sent the port 2 back to the default.. my problem is at first i could connect with no problems, i went to plc mode and changed acouple things. trying to make the plc work for modbus. well for some reason i changed the address to 5 i belive but not sure. now i get the can not connect to plc. I have tried a lot the connection says disabled in yellow.. anyone help???
its a DL06