adccommunitymod (AutomationDirect) asked a question.
How to reset EBC errors
Created Date: December 05,2005
Created By: rex2802
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
When I powerdown and restore power or unplug/plug the Ethernet cable from any of my 4 EBC's the fault bits (x300-x303) will not reset. I have to go into NetEdit3 to clear them. All EBC's and the ERM have the latest firmware. The errors are 121, which is a power error and I also get a communication timeout.
Created Date: December 21,2005
Created by: stimpsonjcat
Page 4-16 of the ERM manual details resetting slaves.
http://web6.automationdirect.com/static/manuals/h24ermm/h24erm_m.pdf
Created Date: March 16,2006
Created by: rex2802
I have tried the examples in the manual, but cannot still cannot reset the faults.
I can inhibit the EBC 'c but X330 never comes ON. The manual example mentions resetting Terminator I/O modules. I am using the H2-EBC in standard racks.
Sometimes I can clear the error by a power cycle to the faulted rack. Most times I can only reset the fault by using ERM workbench.
I must be over looking something.
Created Date: March 20,2006
Created by: GKiser
The errors should clear when:
(1) The actual error situation has gone away, and...
(2) You read the error status from the ERM using ladder logic.
Are you doing this and the bits are still not clearing?
Created Date: March 21,2006
Created by: rex2802
The error exists in the PLC Input (X300-X303) assigned to the respective EBC module. The EBC module error LED is OFF, but the I/O isn't updated in the EBC.
I end up going resetting the error using ERM Workbench. That's the only way I 've been able to clear the error bit. (X300-X303). The error shows up Yellow in ERM not Red. I haven't figured it out yet.
Created Date: March 21,2006
Created by: franji1
First, what is causing the error? Is the ERM's watchdog firing? You may need to enable the Pet frequency in the ERM configuration (set it to HALF the Watchdog value). If it's not a timeout, what is the error and what is causing the error?
We messed up in the ERM workbench when we ENabled the watchdog timer, but DISabled petting it, by default. We forgot that runtime edits will cause the ERM watchdog to fire just about EVERY time and cause an error. You can change that in your ERM config and in the "default " config for any future ERM configuration (see View->Options). In the Options dialog, the Slave Defaults section, set the Pet Frequency equal to half the Watchdog value.
Also, make sure your watchdog timer value is at least twice your typical scan time, but at least 250 ms (it doesn't help too much to make it fast - it just causes more errors). Do you have LONG PLC scan times? Then this may causing the problem???
You reset the slave by disabling it, then reenabling it as simpsonjcat pointed to page 4-16 of the ERM manual. You must have the right Y address based off your ERM configuration. These "disable bits " take up the first 16 bits of the "discrete output " map. The ERM must recognize the Y value to be ON, then turn it OFF. This may take multiple PLC scans, hence the need to monitor X330 (in the manual's example) to know when it is "done " disabling a slave.
Make sure YOUR Y address and YOUR X address are the right ones in your "reset slave " logic
Created Date: March 22,2006
Created by: rex2802
The error (slave not responding) can be caused by unplugging the EBC or when the rack is powered down and then back on.
If the slave Watchdog timeout is Disabled the following occurs. I unplug the ethernet cable, X303 goes ON. When I reconnect the Ethernet cable the X303 goes OFF. If the Watchdog timer is Enabled, 250 MS, and ERM Pet Frequency is 125 ms, replugging in the Ethernet cable will NOT reset X303.
My scan times during this test was 21 ms, max = 24. During machine operation 60-80 ms are typical.
I can disable the EBC by forcing Y303 OFF. The modules Error light goes on. Turning Y303 OFF clears the error light.
All 4 of my slaves will show their repective faults (X300-X303) if powered down and then up. ERM Workbench reports "slave not responding " yet the activity light on the EBC will show activity, and the inputs will reflect the true input status and I can energize outputs. But the fault bit will be on. At this point I think there is an hardware issue here with being able to disable and re-enable the EBC to clear reset the fault bit.
Adjusting,enabling,disabling watchdog timers and pet frequency haven't helped resolve this issue.
I may have to remove the logic that signals the operator that a rack is faulted at this point since I haven't been able to resolve this issue.
Created Date: March 22,2006
Created by: franji1
Based on your description, you are doing exactly what you need to do - and it should behave as you think it should (but it's not - hmmmmm).
Please email support@hosteng.com and hopefully we can figure this out!!
Created Date: March 22,2006
Created by: rex2802
I will send an email. I use AD products exclusively because of there ease of use and reliability. Usually any questions I have get answered here or I work through them.
This one has me puzzled.
Thanks!
Created Date: December 05,2005
Created by: rex2802
When I powerdown and restore power or unplug/plug the
Ethernet cable from any of my 4 EBC's the fault bits (x300-x303) will not reset. I have to go into NetEdit3 to clear them. All EBC's and the ERM have the latest firmware.
The errors are 121, which is a power error and I also get a communication timeout.