adccommunitymod (AutomationDirect) asked a question.
OPC Client w/KEP getting unknown C,V,T... values
Created Date: October 06,2005
Created By: BrewMaster
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Im using KEPDirect for PLC's and i have a device and channel setup. I then open the OPC Quick client to test my communication and my system and channel variables are good. But my device variables such as my Contacts, V-Memory... all say Quality is bad and Value is Unknown. I'm using H0-ECOM with an D0-06. I can link up the D0-06 with my Directsoft32 software just fine with the ECOM module so my cableing should be OK.
Created Date: October 13,2005
Created by: stimpsonjcat
Older version of Kep?
Created Date: October 06,2005
Created by: BrewMaster
Im using KEPDirect for PLC's and i have a device and channel setup. I then open the OPC Quick client to test my communication and my system and channel variables are good. But my device variables such as my Contacts, V-Memory... all say Quality is bad and Value is Unknown. I'm using H0-ECOM with an D0-06. I can link up the D0-06 with my Directsoft32 software just fine with the ECOM module so my cableing should be OK.