adccommunitymod (AutomationDirect) asked a question.

OPC Client w/KEP getting unknown C,V,T... values

Created Date: October 06,2005

Created By: BrewMaster

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Im using KEPDirect for PLC's and i have a device and channel setup. I then open the OPC Quick client to test my communication and my system and channel variables are good. But my device variables such as my Contacts, V-Memory... all say Quality is bad and Value is Unknown. I'm using H0-ECOM with an D0-06. I can link up the D0-06 with my Directsoft32 software just fine with the ECOM module so my cableing should be OK.


  • adccommunitymod (AutomationDirect)

    Created Date: October 13,2005

    Created by: stimpsonjcat

    Older version of Kep?

  • adccommunitymod (AutomationDirect)

    Created Date: October 06,2005

    Created by: BrewMaster

    Im using KEPDirect for PLC's and i have a device and channel setup. I then open the OPC Quick client to test my communication and my system and channel variables are good. But my device variables such as my Contacts, V-Memory... all say Quality is bad and Value is Unknown. I'm using H0-ECOM with an D0-06. I can link up the D0-06 with my Directsoft32 software just fine with the ECOM module so my cableing should be OK.

    Expand Post