adccommunitymod (AutomationDirect) asked a question.

MDM-TEL modem

Created Date: September 26,2004

Created By: awalinski

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Can PC with a KEPDirect on it poll data from remote plc connected to a modem? Can I send any data TO plc through this modem?


  • adccommunitymod (AutomationDirect)

    Created Date: September 27,2004

    Created by: Tech Guy

    Can PC with a KEPDirect on it poll data from remote plc connected to a modem?

    Yes, modems are supported with KepDirect.

    Can I send any data TO plc through this modem?

    KepDirect supports bidirectional data transfers, so depending on the application that you will be using it could be able to write data to the plc.

    Of course as always, modem use depends on the quality of the phone lines.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 07,2009

    Created by: amcbrearty

    Where to start?

    I have DSData Server on my system and I am able to download to Excel when connected directly to the PLC.

    If I connect via a Modem using using DirectSoft to establish the modem link, I can then start DSData and update my v-register data in Excel.

    If I connect to the Modem using Hyperterminal (Windows XP). I can start DSData and the values seem to update when I start Excel, however the spreadsheet does not update.

    SO, what I'd _really_ like to do is to simply start Excel, and have it start DSData (it knows it needs to) _and_ dial up the modem connection.

    If that is not possible, I would be OK with starting DSData, then Excel, but I see no way to connect to a modem from DSData. In directsoft, you can simply click the link and it dials the modem and starts communications.

    thanks,

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 16,2009

    Created by: stimpsonjcat

    If you start Excel, and it needs DSDATA, it will start it.

    If DSDATA needs data from a modem link, it will dial it.

    But I think there were some nasty bear traps if trying to use modems to multiple devices with DSDATA, I think there is likely a FAQ on it at the Host site.

  • adccommunitymod (AutomationDirect)

    Created Date: February 17,2009

    Created by: amcbrearty

    If you start Excel, and it needs DSDATA, it will start it.

    If DSDATA needs data from a modem link, it will dial it.

    But I think there were some nasty bear traps if trying to use modems to multiple devices with DSDATA, I think there is likely a FAQ on it at the Host site.

    THANKS!!! Amazing! It worked, but I had to add the executable path so that it found DSData.exe.

    It is so obvious, now. When I started Excel, it never could find DSData.exe before, so I put the folder that DSData sits in as one of the $PATH variable on the system. It started DSData, & dialed the modem...

    This is so much simpler than what I had been doing! Thanks again!

    --now, on a similar note--

    Does this same procedure work with KEPDirect for PLCs? When I open a spreadsheet that can talk to KepDirect, it looks for a program called "KEPDIREC.EXE ". The executable is called "ServerMain.exe " in KepDirect.

    Assuming this works the same way that DSData works, how do you get KEPDirect to startup when Excel is looking for it?

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 30,2009

    Created by: stimpsonjcat

    Just like DSDATA, if Excel requests data from Kep, it ought to start.

    Having said that, the intent of being able to run KEP as a service is to obviate this requirement by having it always running.

  • adccommunitymod (AutomationDirect)

    Created Date: September 26,2004

    Created by: awalinski

    Can PC with a KEPDirect on it poll data from remote plc connected to a modem?

    Can I send any data TO plc through this modem?