adccommunitymod (AutomationDirect) asked a question.

305 ethernet communications

Created Date: October 07,2003

Created By: Matt Pawlak

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is there a reason there is no ethernet communications module for the 305 series PLC? If there are no hardware limitations, when might we see a H3-ECOM module? I could live with it only being able to function with a 350 CPU. In the meantime, has anyone worked around this? What's my best bet? Slap a DL05 onto the panel to connect to the ethernet and use its serial port to communicate with the DL350?


  • adccommunitymod (AutomationDirect)

    Created Date: October 08,2003

    Created by: franji1

    The 305 backplane hardware does not support intelligent modules very well (330/340 limitations and speed issues).

    HOWEVER, from a cost standpoint, buy a $99 05 and an H0-ECOM for another $169, that's just $268 - not bad for an "H3-ECOM "!!

    Port 2 on the 05 can master to a slave 330/340/350 via DirectNet protocol using RX/WX instructions in the 05. The 330 would require a DCU module (if you didn't already have one), but the 340 and 350 have built in DirectNet slave support!

    Sounds like a good solution to me!?!

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: October 08,2003

    Created by: Matt Pawlak

    Yes, that sounds like an acceptable workaround. Thanks!

  • adccommunitymod (AutomationDirect)

    Created Date: October 07,2003

    Created by: Matt Pawlak

    Is there a reason there is no ethernet communications module for the 305 series PLC? If there are no hardware limitations, when might we see a H3-ECOM module? I could live with it only being able to function with a 350 CPU.

    In the meantime, has anyone worked around this? What's my best bet? Slap a DL05 onto the panel to connect to the ethernet and use its serial port to communicate with the DL350?

    Expand Post