adccommunitymod (AutomationDirect) asked a question.

SOLO Controllers for Open Loop Control

Created Date: January 06,2016

Created By: paulreeder

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hello All- At our food plant, we often use Open Loop Temperature control (No temperature feedback). In the past, we used mechanical Eagle Signal & ATC "Percentage Timers ", where, with a fixed time period (30 seconds worked for us), the output could be set to turn on a percentage of the 30 seconds. Set at 50%, the output would be on for 15 seconds & off 15 seconds. Set at 10%, the output would be on for 3 seconds and off 27 seconds. Being mechanical, the % timer life span was about 3 years. Even solid state ATC brand timers would also not last very long. I found nothing for open loop control in the manual or from Tech Support, So I experimented and was able to easily adjust it for open loop control. Take any of the SOLO controllers (Size doesn't matter!) and set as follows: Setup Parameters - PCd0 = 0 Su0 - 0 P0 = 10.0 C0 = 0 d0 = 0 PdoF = 0 HtPd = 10 (Adjust as needed, it's the Time Period, in seconds) tPoF= -4 (Again, adjust as needed to show a PV of 0) Initial Setting Parameters - CnPt = u10 tP-H = 100 tP-L = 0 CtrL = Pcd S-HC = Heat I have only used this for SSR fired heating outputs (SLXXXX-VR), so my time period can be short. Obviously, triggering contactors or other outputs may not be suitable. Good Luck. "May the Control be in your Favor " Ha Ha -Paul Reeder


  • adccommunitymod (AutomationDirect)

    Created Date: January 06,2016

    Created by: paulreeder

    Sorry, but I forgot to add the operation mode. Simply set the SV for 0 (0% output) on up to 100 (100% output), or anything in between.

    -Paul Reeder

  • adccommunitymod (AutomationDirect)

    Created Date: January 06,2016

    Created by: paulreeder

    Hello All-

    At our food plant, we often use Open Loop Temperature control (No temperature feedback). In the past, we used mechanical Eagle Signal & ATC "Percentage Timers ", where, with a fixed time period (30 seconds worked for us), the output could be set to turn on a percentage of the 30 seconds. Set at 50%, the output would be on for 15 seconds & off 15 seconds. Set at 10%, the output would be on for 3 seconds and off 27 seconds.

    Being mechanical, the % timer life span was about 3 years. Even solid state ATC brand timers would also not last very long.

    I found nothing for open loop control in the manual or from Tech Support, So I experimented and was able to easily adjust it for open loop control.

    Take any of the SOLO controllers (Size doesn't matter!) and set as follows:

    Setup Parameters - PCd0 = 0 Su0 - 0 P0 = 10.0 C0 = 0 d0 = 0

    PdoF = 0 HtPd = 10 (Adjust as needed, it's the Time Period, in seconds)

    tPoF= -4 (Again, adjust as needed to show a PV of 0)

    Initial Setting Parameters - CnPt = u10 tP-H = 100 tP-L = 0

    CtrL = Pcd S-HC = Heat

    I have only used this for SSR fired heating outputs (SLXXXX-VR), so my time period can be short. Obviously, triggering contactors or other outputs may not be suitable.

    Good Luck.

    "May the Control be in your Favor " Ha Ha

    -Paul Reeder

    Expand Post