adccommunitymod (AutomationDirect) asked a question.

GS3 Communications with PC and GSoft

Created Date: November 27,2019

Created By: roglc

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I want to use GSoft on the plant floor with the GS Series of drives using RS-485 protocol. In the drive manuals it only mentions two methods each requiring a converter that needs an external 24Vdc power source. Is there a cable converter that will work? Such as the USB-485M?


  • adccommunitymod (AutomationDirect)

    Created Date: November 27,2019

    Created by: roglc

    I want to use GSoft on the plant floor with the GS Series of drives using RS-485 protocol. In the drive manuals it only mentions two methods each requiring a converter that needs an external 24Vdc power source. Is there a cable converter that will work? Such as the USB-485M?