adccommunitymod (AutomationDirect) asked a question.
P2-550 communications to a gs3-22PO
Created Date: January 22,2018
Created By: drheck
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
What is the best way to communicate with a gs3-22PO using a P2-550 PLC?
Created Date: January 22,2018
Created by: drheck
What is the best way to communicate with a gs3-22PO using a P2-550 PLC?
Created Date: January 23,2018
Created by: kewakl
Help topic P200
Have you looked at GS-EDRV100?
First setup the EDRV to match
Then setup your drive in PAC hardware config.
Then use GSR/GSW to read and write from/to the drive.
Disclaimer: I have NOT done this.
Created Date: January 23,2018
Created by: drheck
Thanks for the response. I did see that method, but was wondering if I could just use the rs485 port directly and then use Modbus Read/Write commands (MRX/MWX) from my ladder logic? I have only programmed Allen Bradley PLC's and am trying to learn the world of Automation Direct for a small project I 've taken on...
Created Date: January 23,2018
Created by: g.mccormick
There should be no reason that you cannot use the modbus option via 485. It may be more code work, but saves the cost of the ERDV.
Created Date: January 28,2018
Created by: Ridgeline Mach
Have done it many times, and it works well. But the commands are Modbus Read and Modbus Write in PSuite. Just a word of caution, your writes have to be limited to three registers. Follow chapter 5 of the GS drive manual for help. I use the cable listed for Click port 3. I 've also controlled 3 drives from the same P2K, and a nice feature of the P2K is you can set times for automatic polling in the read and write commands.
Created Date: January 28,2018
Created by: kewakl
Have done it many times, and it works well. ...
Just a word of caution, your writes have to be limited to three registers.
Is this a documented rule or an observed limitation?
Do you know if this applies to other configurations (comms protocol, cable length, net configuration, termination, message length, comms delays, baud...) than what you have used?
I see in CH5 that the CLICK example has three registers in some of the SEND instructions, but that may be coincidence.
Also, in the DL example has three registers in some of the MWX instructions. Again, that may be coincidence.
The only thing that I can find in the manual that says why in the examples they only SEND three registers is respect for the Keypad STOP button:
Separate Run Command Write Instruction
Why do we write the Run Command with a separate write instruction? If we
write the Run Command to the drive along with the Speed Reference, Direction,
External Fault, and Fault Reset Commands, we can keep the parameter addresses
in sequence, and we can update all five of the commands with one write
instruction . This method is valid only if we disable the drive’s keypad STOP
button (P3.00 = 04).
Typically, the keypad STOP button will be enabled (P3.00 = 03), and we need to
prevent a change in one of the other commands from overriding a keypad Stop
Command by causing a previous Run Command to be rewritten to the drive. By
using a separate Run Command write instruction, only a deliberate Run
Command change by the program will run the drive again after a stop.
Created Date: January 28,2018
Created by: Ridgeline Mach
I called tech support when I was having an issue of the drive(s) ignoring my run command, and I was asked "how many " registers was I writing to at once, and I said, "four. " That was when I was told to write to no more than three. So I have one Write for Speed, Run, and Direction, and a 2nd for Drive Reset.
Edit: My Reads are looking at the first eight of the read-only status addresses.
Created Date: January 28,2018
Created by: kewakl
I called tech support when I was having an issue of the drive(s) ignoring my run command, and I was asked "how many " registers was I writing to at once, and I said, "four. " That was when I was told to write to no more than three. So I have one Write for Speed, Run, and Direction, and a 2nd for Drive Reset.
Edit: My Reads are looking at the first eight of the read-only status addresses.
Hmm, If you had only answered the techsupport guy "FIVE ", then your answer may have had merit. J/K
Makes me wonder though, if you had answered FIVE, would you have been negotiated in to trying just FOUR, then THREE, until it worked?
The MANUAL Programming example eludes to being able to write to FIVE registers. we can update all five of the commands with one write instruction .
Created Date: January 29,2018
Created by: Ridgeline Mach
Hmm, unless it's drive dependent. In the application, I was using GS2's.
Created Date: January 29,2018
Created by: kewakl
The GS2 manual has the SAME SENTENCE fragment as the GS3. Ch5 - pg 29
If we write the Run Command to the drive along with the Speed Reference, Direction, External
Fault, and Fault Reset Commands, we can keep the parameter addresses in sequence,
and we can update all five of the commands with one write instruction.