adccommunitymod (AutomationDirect) asked a question.
Created Date: October 16,2014
Created By: vanagsys
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
*** This is on a DL205 series with a 260 CPU Not sure why I put DL06 in the title (too many things going on) I am setting up a control panel that will contain 4 GS3 Drives that I need to control from a C-MORE. The only parameters I need to control via modbus will be speed and fault reset. I want to show amps, motor load and freq. on the cmore. I am controlling the drives individually by an isolated relay card. I have never set up modbus so I have been studying the manual and I understand the v memory addressing and such but I was wondering if anybody on here could give me some examples. Thanks
Created Date: October 16,2014
Created by: bcarlton
The GS3 manual has some examples near the end. It shows the communication hookup. The DL260 provides the MWX and MRX instructions which should make writing the code fairly easy.
Created Date: October 16,2014
Created by: vanagsys
*** This is on a DL205 series with a 260 CPU
Not sure why I put DL06 in the title (too many things going on)
I am setting up a control panel that will contain 4 GS3 Drives that I need to control from a C-MORE. The only parameters I need to control via modbus will be speed and fault reset. I want to show amps, motor load and freq. on the cmore. I am controlling the drives individually by an isolated relay card. I have never set up modbus so I have been studying the manual and I understand the v memory addressing and such but I was wondering if anybody on here could give me some examples.
Thanks