adccommunitymod (AutomationDirect) asked a question.

System Design with Do-More

Created Date: January 24,2013

Created By: ksmith

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Trying to design a system and need some help from the great minds of the forum. I have 4 panels to build: A, B, C, and D. Panel A will be the "master " with a Do-More CPU, an ERM, and a 12 " C-More. Panel B will have an EBC100 and some discrete I/O. Panel C will have an EBC100 and some discrete I/O. Panel D will have an EBC100, (2) GS2 Drives, and some discrete I/O. Here is where I am at a loss: 1. I need a C-More Micro at each of the panels B, C, and D. They could be more than 50 feet from Panel A. Should I use an FA-ISOCON at each panel for the C-More Micros and chain them together from the D-More? 2. I also normally control/monitor the GS2 drives via RS485. No RS485 if I use an EBC. Any Pro/Con to using an GS-EDRV100 for the GS2 drives instead of RS485?? Thanks for your time and knowledge.


  • adccommunitymod (AutomationDirect)

    Created Date: January 24,2013

    Created by: Do-more PE

    1. Cmore Micros cannot be daisy chained since they are a mastering device. Only one master on a network. You would need to use FA-ISOCONs and H2-SERIO or H2-SERIO-4 cards.

    2. I would hang the EDRV's off of the ERM. Problem solved.

  • adccommunitymod (AutomationDirect)

    Created Date: January 24,2013

    Created by: ksmith

    Trying to design a system and need some help from the great minds of the forum. I have 4 panels to build: A, B, C, and D.

    Panel A will be the "master " with a Do-More CPU, an ERM, and a 12 " C-More.

    Panel B will have an EBC100 and some discrete I/O.

    Panel C will have an EBC100 and some discrete I/O.

    Panel D will have an EBC100, (2) GS2 Drives, and some discrete I/O.

    Here is where I am at a loss:

    1. I need a C-More Micro at each of the panels B, C, and D. They could be more than 50 feet from Panel A. Should I use an FA-ISOCON at each panel for the C-More Micros and chain them together from the D-More?

    2. I also normally control/monitor the GS2 drives via RS485. No RS485 if I use an EBC. Any Pro/Con to using an GS-EDRV100 for the GS2 drives instead of RS485??

    Thanks for your time and knowledge.

    Expand Post