adccommunitymod (AutomationDirect) asked a question.
Differences Between GS2 & GS3 Drives
Created Date: December 13,2011
Created By: dieseltwitch
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I'm trying to pin down the major difference between the two drive types. they are both Volts/Hertz Type drives but the GS3 is 55$ more for a 1HP drive? the only major difference i can see is the the option to add an encoder. is that all? and it even looks like the GS3 doesn't have a variable carrier frequency on all models. I'm confused...
Created Date: December 13,2011
Created by: Do-more PE
The GS3 is a sensorless vector drive and the keypad is much more advanced.
The GS2 is Volts/Hertz only.
Created Date: December 14,2011
Created by: dieseltwitch
Noted, Thanks
Created Date: December 13,2011
Created by: dieseltwitch
I'm trying to pin down the major difference between the two drive types. they are both Volts/Hertz Type drives but the GS3 is 55$ more for a 1HP drive? the only major difference i can see is the the option to add an encoder. is that all? and it even looks like the GS3 doesn't have a variable carrier frequency on all models.
I'm confused...