adccommunitymod (AutomationDirect) asked a question.
Reverse Command GS2
Created Date: October 07,2008
Created By: gbradley
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
How do I set up a GS2 so that if the Reverse command is set, it will only run in Jog mode? I don't want them to be able to increase the speed in Reverse. Are there examples somewhere?
Created Date: October 07,2008
Created by: gbradley
Is there a place here with examples?
This is what I came up with P3.01 set to 02.
Will this work?
Thanks http://forum.automationdirect.com/attachment.php?attachmentid=52&d=1223408653
Created Date: October 08,2008
Created by: milldrone
George,
There may be a problem with the sequence of contacts. I tried something similar to this a while back.
The manual states: "Note: The Jog Command cannot be used when the motor is running. The motor must be stopped to initiate this command. ".
What I'm remembering was that if your jog button was pressed first it would use the jog speed reference. But if it received the run command first then what ever the speed reference was it would use that.
Edit: My newest manual says "Note: the motor must be stoped to initate this command. The jog command cannot be used simultaneously with an active FWD?STOP, REV/STOP command. The jog command can be used with an active REV/FWD command. " Page 4-25
If I'm remembering correctly I just used one of the preset speeds in combination with the reverse selection
Created Date: October 08,2008
Created by: gbradley
Thanks Vaughn,
I will try that and remember to post my results if anyone is interested.
Thanks
Created Date: October 08,2008
Created by: milldrone
I will try that and remember to post my results if anyone is interested.
George, please do.
A couple of things appear to be different between your application and mine. It looks like you are planning to 100% hardwire the controls and take advantage of the built in "3 wire scheme ". I was replacing a yaskawa with a GS2. I also had a PLC hooked up to the inputs and they were in the "2 wire mode ". In the Yaskawa the "jog " input took precedence over all other inputs except "Base Block ". So the PLC programming took advantage of that. When I fired up the GS2 it would not go into "jog " every time, quite a puzzler until I found the info on the GS2 "jog ".
Created Date: October 07,2008
Created by: gbradley
How do I set up a GS2 so that if the Reverse command is set, it will only run in Jog mode?
I don't want them to be able to increase the speed in Reverse.
Are there examples somewhere?