adccommunitymod (AutomationDirect) asked a question.
Created Date: November 05,2006
Created By: atfab
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I have a machine that uses a DLo5 , gs1 and a optimate 0p-414 to set timer and counter set points . I need the 4x protection, to much opening the pannel to change settings the drive switches between 2 multi-speed settings each cycle and these need to be changed for different products. what is the best way to remote change 5-02 , 5-03? I have extra room in my op414 can I use the top port on the DLo5 to communicate with the gs1 if so what has to be changed to allow programing? can I use an input to change ladder for program/run? would switching to a c-more micro help?
Created Date: November 05,2006
Created by: atfab
I have a machine that uses a DLo5 , gs1 and a optimate 0p-414 to set timer and counter set points . I need the 4x protection,
to much opening the pannel to change settings
the drive switches between 2 multi-speed
settings each cycle and these need to be changed for different products. what is the best way to remote change 5-02 , 5-03?
I have extra room in my op414 can I use the top port on the DLo5 to communicate with the gs1
if so what has to be changed to allow programing? can I use an input to change ladder for program/run?
would switching to a c-more micro help?