adccommunitymod (AutomationDirect) asked a question.

GS3 drive multiple inputs

Created Date: May 19,2006

Created By: lundell

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is it possible to control a GS-3 with both a GS-EDRV and a seperate controller with 0-10 volt output to the drive. I know that you have to set the parameter P3.00 for operation command but is there a way to have a "manual operation " controled by a touch screen via ethernet and an "automatic operation " controlled by the 0-10 volt on the control terminals.


  • adccommunitymod (AutomationDirect)

    Created Date: May 19,2006

    Created by: lundell

    Is it possible to control a GS-3 with both a GS-EDRV and a seperate controller with 0-10 volt output to the drive. I know that you have to set the parameter P3.00 for operation command but is there a way to have a "manual operation " controled by a touch screen via ethernet and an "automatic operation " controlled by the 0-10 volt on the control terminals.