adccommunitymod (AutomationDirect) asked a question.

Click Node

Created Date: December 16,2014

Created By: mwdkmpr

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is there a way to change the node address of a click; other than with the programing software?


  • adccommunitymod (AutomationDirect)

    Created Date: December 16,2014

    Created by: Do-more PE

    Unfortunately no, Mike.

  • adccommunitymod (AutomationDirect)

    Created Date: December 16,2014

    Created by: Tinker

    While not nearly as easy as, say, a DIP switch, If your primary concern is not wanting the end user/installer to be messing with the program software, it is possible (but I'm not 100% sure) that using the "CLICK loader " could be an option. You'd still have to use the programing software to configure the node number, export the loader file and send it to the end user, and the end user would have to have a PC the loader program (free download) and a proper cable, but they would only have the encrypted loader file and no ability to see or change the source code.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: December 16,2014

    Created by: mwdkmpr

    Is there a way to change the node address of a click; other than with the programing software?