adccommunitymod (AutomationDirect) asked a question.
Displaying Counter Value From CLICK to C-more
Created Date: May 24,2012
Created By: eliw03
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello, I'm setting up a CLICK PLC and C-More EA1-S3MLW HMI. I would like to be able to display the current value of a counter (CTD) on the HMI. When setting it up in the HMI, I do not see a memory address for CTD. Is there an alternate method? Am I missing something? Thank you.
Created Date: May 24,2012
Created by: Do-more PE
Select "Unsigned Integer 32 " for the data type and the CTD value should show up in the drop down.
Created Date: May 24,2012
Created by: eliw03
Select "Unsigned Integer 32 " for the data type and the CTD value should show up in the drop down.
I tried that and the only value that was available was DD.
Created Date: May 24,2012
Created by: eliw03
I tried that and the only value that was available was DD.
It worked with Signed integer 32
Thanks
life saver!!
Created Date: June 06,2012
Created by: kgreen02
eliw, I ran into this same issue, and the signed integer displayed a - before the number. A way around this is to put your CTD value as the source in a single copy box, and select DD1 as the destination. Make the c-more tag as unsigned 32, then you'll lose the -..
Created Date: May 24,2012
Created by: eliw03
Hello,
I'm setting up a CLICK PLC and C-More EA1-S3MLW HMI. I would like to be able to display the current value of a counter (CTD) on the HMI.
When setting it up in the HMI, I do not see a memory address for CTD. Is there an alternate method? Am I missing something?
Thank you.