adccommunitymod (AutomationDirect) asked a question.
Created Date: December 20,2011
Created By: zener
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello, I have the Click C0-02DR-D Analog CPU and I would like to do an experiment where I would feed the current from analog output DA1I (DA1 address DF3) into analog input AD1I (AD1 address DF1) so I can test out my 4” touch panel, adjust the graphics accordingly, and to just get a feel of how things work. The problem I’m having is figuring out how to wire DA1I to AD1I. I have followed wiring from chapter 2 of the CPU manual but the analog input shows 20ma, regardless of the outputs setting. The output works fine, verified by DMM. Any advise would be greatly appreciated! Thanks
Created Date: December 20,2011
Created by: Do-more PE
The 0-20ma inputs and outputs cannot be connected together. You might get away with using the voltage inputs and outputs though.
Created Date: December 20,2011
Created by: zener
Hello,
I have the Click C0-02DR-D Analog CPU and I would like to do an experiment where I would feed the current from analog output DA1I (DA1 address DF3) into analog input AD1I (AD1 address DF1) so I can test out my 4” touch panel, adjust the graphics accordingly, and to just get a feel of how things work. The problem I’m having is figuring out how to wire DA1I to AD1I. I have followed wiring from chapter 2 of the CPU manual but the analog input shows 20ma, regardless of the outputs setting. The output works fine, verified by DMM. Any advise would be greatly appreciated!
Thanks