adccommunitymod (AutomationDirect) asked a question.

Click port to use withCmoreMicro

Created Date: August 03,2012

Created By: Tubecut

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

In the C0-USER-M manual it shows that the CMore micro can be connected to either Port1 or Port2 of the Click. Is this correct? I was thinking that the Click Port1 did not support RTS. Note: I placed a similar question to Tech Suppoort email and then realized that it is the week end.


  • adccommunitymod (AutomationDirect)

    Created Date: August 03,2012

    Created by: Adisharr

    I 've never used port 1 for anything other than programming. Port 2 should work fine.

  • adccommunitymod (AutomationDirect)

    Created Date: August 03,2012

    Created by: Do-more PE

    It is correct. Any of the ports on a Click can be connected to an HMI.

  • adccommunitymod (AutomationDirect)

    Created Date: August 04,2012

    Created by: Tubecut

    Much thanks:)

  • adccommunitymod (AutomationDirect)

    Created Date: August 03,2012

    Created by: Tubecut

    In the C0-USER-M manual it shows that the CMore micro can be connected to either Port1 or Port2 of the Click.

    Is this correct?

    I was thinking that the Click Port1 did not support RTS.

    Note: I placed a similar question to Tech Suppoort email and then realized that it is the week end.