adccommunitymod (AutomationDirect) asked a question.
Created Date: August 19,2014
Created By: DuctSoup
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hi, I'm working on a process water polishing skid and I need a couple CPVC mixing valves (1 " to 2 ", water, ambient to 150F, 100psi @ 10gpm) I can interface with an analog Click PLC at a reasonable price since there will be more than a couple of these in the final system. Modulated would be the most convenient but if floating fail in place, proportional or something else will be significantly less expensive I'm fine with writing some extra code. Does anyone have a recommendation for a manufacturer? Thanks, Craig
Created Date: August 28,2014
Created by: pkshaver
I think Belimo offers PVC valves. I know they have something that would work - not sure how the price will work out.
Created Date: August 28,2014
Created by: Medius
http://www.valworx.com/category/pvc-ball-valves
or
bitorq.com
My application is a very budget conscious one that requires the brass 1 " valve. After searching and searching, these two brands are the most bang for my buck. Not sure if it is your solution with PVC valves, but it would be a good starting point.
Created Date: August 19,2014
Created by: DuctSoup
Hi,
I'm working on a process water polishing skid and I need a couple CPVC mixing valves (1 " to 2 ", water, ambient to 150F, 100psi @ 10gpm) I can interface with an analog Click PLC at a reasonable price since there will be more than a couple of these in the final system.
Modulated would be the most convenient but if floating fail in place, proportional or something else will be significantly less expensive I'm fine with writing some extra code.
Does anyone have a recommendation for a manufacturer?
Thanks, Craig