adccommunitymod (AutomationDirect) asked a question.
Created Date: July 16,2011
Created By: Tubecut
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am attaching a PNG file and also the ckp ladder program. A very simple program ( 2 rungs). I have a timer (T1) that the enable rung has two conditions (AND) , C10 and Not T1 (see png file or the ladder program attached). The problem is that enabling the timer by turning ON C10 the timer runs as expected. If I turn OFF C10, the timer continues to increment TD1. I am using only the monitor on line mode and turning ON/OFF C10 using the over write edit mode in the monitor. Question: Is this a bug in the monitor/edit mode or some other bug? Also, in another short test program (file not attached) I had a rung enabled on First Scan to copy a value to DS1. I was unable to edit/change the DS1 value using the monitor edit mode . Thanks in advance for any input. I am thinking that perhaps I am doing something incorrect here but can't 'see ' it :o I am delaying installing the current version (1.31) for the time being. I was hoping to hear some users comments on 1.31 Once again, thanks for any help
Created Date: July 16,2011
Created by: bcarlton
T1 - you have chosen an OFF DELAY TIMER which times when the input conditions are false.
Created Date: July 17,2011
Created by: Tubecut
Solved
Thanks Bernie. I haven't used the off delay timer often.
The devils in the details :)
Created Date: July 16,2011
Created by: Tubecut
I am attaching a PNG file and also the ckp ladder program.
A very simple program ( 2 rungs). I have a timer (T1) that the
enable rung has two conditions (AND) , C10 and Not T1
(see png file or the ladder program attached).
The problem is that enabling the timer by turning ON C10 the
timer runs as expected. If I turn OFF C10, the timer continues
to increment TD1.
I am using only the monitor on line mode and turning ON/OFF
C10 using the over write edit mode in the monitor.
Question: Is this a bug in the monitor/edit mode or some other bug?
Also, in another short test program (file not attached) I had a rung enabled on First Scan to copy a value to DS1.
I was unable to edit/change the DS1 value using the monitor
edit mode .
Thanks in advance for any input. I am thinking that perhaps I am doing something incorrect here but can't 'see ' it :o
I am delaying installing the current version (1.31) for the time being. I was hoping to hear some users comments on 1.31
Once again, thanks for any help