adccommunitymod (AutomationDirect) asked a question.

Click - Port Forwarding

Created Date: December 14,2015

Created By: kewakl

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

post 18 ] I cannot successfully complete the Port Forwarding demo in the video . I have a Cisco Linksys E2500 router. - As close as I could get to the router from the demo. Router WAN 192.168.7.1 Router LAN 192.168.1.1 I have a WinXP laptop for router config 192.168.1.100 I have a Win7 laptop for Click programming 192.168.7.231 I have a CLICK C0-10DRE-D IP 192.168.1.11 Gateway 192.168.1.1 (router LAN IP) From either laptop, I can ping the respective router network connections. From the WinXP laptop, I can ping the CLICK at .1.11 From the Win7 laptop, I cannot connect to the CLICK through the router. I get Error PTC-007 'Cannot connect to the PLC ' Other than exact IP addresses as used in the video, minor differences in router model and firmware differences and a single CLICK, I have copied the steps in the video. In following posts, I will include screen shots of the router setup pages.


  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2015

    Created by: kewakl

    In the Setup-Basic Setup screenshot, you can see the WAN/LAN IP setup.

    In the video, the narrator said that his router required the Gateway settings.

    My router complains about empty DNS 1 .

    In the Security-Firewall screenshot, I have the IPv6 and IPv4 SPI Firewall disabled.

    In the demo, the IPV4 and IPv6 were not broken out as individual settings

    Also, I have disabled the Filter Anonymous Internet Requests.

    In the Wireless-BasicWireless screenshot, I have disabled the 2.5GHz and 5GHz capability.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2015

    Created by: kewakl

    IN the AppsGaming screenshot, I have the same port configuration as CLICK1 in the video.

  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2015

    Created by: kewakl

    I can do the respective pings to the router.

  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2015

    Created by: kewakl

    Any suggestions are appreciated.

  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2015

    Created by: Do-more PE

    Make sure your Click port setup has the router IP address (192.168.1.1) for the gateway setting.

    Be sure that you are pointing the Click software at port 5555 when adding the Outside network link.

  • adccommunitymod (AutomationDirect)

    Created Date: December 14,2015

    Created by: kewakl

    Make sure your Click port setup has the router IP address (192.168.1.1) for the gateway setting.

    Will check in the morning!

    It is.

    Be sure that you are pointing the Click software at port 5555 when adding the Outside network link.

    I know that I have done this.

    Thanks Do-More PE!

    Still errors out --- PTC-007 - cannot connect

    Have attempted this with firewall disabled - no connection.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: December 15,2015

    Created by: jackson

    Do you have multiple Network Interfaces on the PC trying to connect to CLICK on the WAN side of the router (192.168.7.xxx)?

    What is the IP address and subnet mask of the other interfaces?

    I would disable any other interfaces for troubleshooting purposes.

  • adccommunitymod (AutomationDirect)

    Created Date: December 15,2015

    Created by: kewakl

    Do you have multiple Network Interfaces on the PC trying to connect to CLICK on the WAN side of the router (192.168.7.xxx)?

    What is the IP address and subnet mask of the other interfaces?

    I would disable any other interfaces for troubleshooting purposes.

    Do you have multiple Network Interfaces on the PC trying to connect to CLICK on the WAN side of the router (192.168.7.xxx)?

    No, only the laptop WIRED ethernet

    What is the IP address and subnet mask of the other interfaces?

    n/a

    I would disable any other interfaces for troubleshooting purposes.

    I did disable the silly USB Dock ethernet and the wireless connection. Still cannot connect to the CLick thru the router.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: December 15,2015

    Created by: jackson

    Can you wireshark on the inside of the router (from the router to the CLICK PLC)?

    I would, as a test, change the external port on the router setup to make it the same as the inside: 25425.

    Try to isolate whether the problem is a router issue or not. Routers are quirky on the best of days...

  • adccommunitymod (AutomationDirect)

    Created Date: December 15,2015

    Created by: kewakl

    I cannot Wireshark anytime soon.

    Tested changing the port number from 5555 to 25425 - still no connection.

    Will see if my IT guy has another router - preferably the same E1000 as in demo.

    I'll also try to get him involved.

    I will post if I make progress..

    Thank you for your input.

    Expand Post
10 of 19