adccommunitymod (AutomationDirect) asked a question.

Apple version of Click Software

Created Date: January 09,2013

Created By: lonewolf32

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Is there a Apple version of the click Software?


  • adccommunitymod (AutomationDirect)

    Created Date: January 09,2013

    Created by: Do-more PE

    Unfortunately, no.

  • adccommunitymod (AutomationDirect)

    Created Date: January 14,2013

    Created by: Do-more PE

    That or Boot Camp. Either one would allow Windows to Run on the Apple machine.

  • adccommunitymod (AutomationDirect)

    Created Date: January 24,2013

    Created by: JoeW

    There is a free program called Wineskin that can be used to port Windows software to Mac, but it is typically for games. It isn't extremely difficult to use, and may be worth a shot in attempting to port it yourself. That being said, games don't typically require direct access to a USB port or Ethernet port.

  • adccommunitymod (AutomationDirect)

    Created Date: January 25,2013

    Created by: dieseltwitch

    I 've been having this same problem for years. lol. I just run a very small trimed version of windows in parallels. works pretty good alot of the VM's dont seam to work well when connection to the PLC. Parallels is the only one I 've found that works 100% of the time.

    I also just picked up a dirt cheap 300$ laptop for programming and service calls

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 09,2013

    Created by: lonewolf32

    Is there a Apple version of the click Software?