adccommunitymod (AutomationDirect) asked a question.
Created Date: November 12,2017
Created By: GlennLee
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
My customer bought the BX-DM1E-36ED23-D controller because he was told by A-D that it had eight High-Speed Outputs. When I received the project information and tried to configure the High-Speed outputs, I discovered that Axis0 is a "virtual " axis and does not allow me to assign actual outputs to it. I configured the remaining axes to outputs, leaving one pair of outputs for...what exactly? In other words, I have four axes and eight outputs, but no way to actually use one of the axes to control a stepper controller. Why does Axis0 exist?
Created Date: November 12,2017
Created by: GlennLee
My customer bought the BX-DM1E-36ED23-D controller because he was told by A-D that it had eight High-Speed Outputs. When I received the project information and tried to configure the High-Speed outputs, I discovered that Axis0 is a "virtual " axis and does not allow me to assign actual outputs to it. I configured the remaining axes to outputs, leaving one pair of outputs for...what exactly?
In other words, I have four axes and eight outputs, but no way to actually use one of the axes to control a stepper controller. Why does Axis0 exist?
Created Date: November 12,2017
Created by: kewakl
According to BobO: Axis0 is a purely virtual axis that is there solely for the purpose of driving the other axes in AXCAM, AXFOLLOW, and AXGEAR instructions.
https://forum.automationdirect.com/forum/give-us-your-2-cents/105237-brx-team-we-need-1-more-motion-instruction-please?p=106557#post106557
Created Date: November 12,2017
Created by: BobO
There are three physical axes, hardware based pulse outputs. We added a fourth software only axis to allow the three physical axes to be slaved to it, rather than forcing you to burn a physical axis for mastering. That's very convenient when doing three axis coordinated moves.
Created Date: November 12,2017
Created by: BobO
There are a total of 8 high speed outputs, but they exist for all high speed output functions including PWMs, TDOs, and pulse outputs. High speed outputs can also be driven from interrupts.
Created Date: November 12,2017
Created by: GlennLee
So...I could use the fourth set of outputs for a slave to Axis0 using AXFOLLOW? That would allow me to have the four outputs I need. Otherwise, I need to have my customer return all of the components they ordered for a BRX-based project and substitute a 205-series DoMore with CTRIO2s.
Created Date: November 12,2017
Created by: BobO
So...I could use the fourth set of outputs for a slave to Axis0 using AXFOLLOW? That would allow me to have the four outputs I need. Otherwise, I need to have my customer return all of the components they ordered for a BRX-based project and substitute a 205-series DoMore with CTRIO2s.
A single BRX unit can drive three steppers. If you need a fourth, you will either need to add a second BRX as an axis controller, or yes, you will have to replace the BRX system with a 205 and two CTRIO2s. If the motion moves are fairly simple, I personally would add the 2nd BRX, since I like the motion interface more than the CTRIO2.