adccommunitymod (AutomationDirect) asked a question.

Do-More not reading all GS1 Status Addresses over RS485

Created Date: January 16,2016

Created By: Frontier

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I currently have 5 GS1 drives controlled by a H2-DM1E unit with a SERIO-4 module. Control works perfectly, as do most of the status addresses (I have no problem reading current RPM, output current, etc.), except for address 48460 (% load). This always shows as zero when the drive is running. This is my MRX box for one of the drives: 1939 After trying a few things with the different drives, it appears that % load is actually being placed in the address for firmware version on the drive. I 've tried loading the address as part of a range, as well as individually, and get the same result. Has anyone else experienced this? Also, I'd attach my drive firmware revision, but I'm offsite and due to this issue can't read it off the PLC.


  • adccommunitymod (AutomationDirect)

    Created Date: January 16,2016

    Created by: Frontier

    I currently have 5 GS1 drives controlled by a H2-DM1E unit with a SERIO-4 module. Control works perfectly, as do most of the status addresses (I have no problem reading current RPM, output current, etc.), except for address 48460 (% load). This always shows as zero when the drive is running.

    This is my MRX box for one of the drives:

    1939

    After trying a few things with the different drives, it appears that % load is actually being placed in the address for firmware version on the drive. I 've tried loading the address as part of a range, as well as individually, and get the same result. Has anyone else experienced this?

    Also, I'd attach my drive firmware revision, but I'm offsite and due to this issue can't read it off the PLC.

    Expand Post