adccommunitymod (AutomationDirect) asked a question.
windows 10
Created Date: August 01,2015
Created By: gringogreg
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Have there been any issues yet with any AD software running on windows 10 DS6, DoMore designer, CMore micro, etc.
Created Date: August 02,2015
Created by: DonHill
P2000 ok with Win 10
Carried over a new egg picker program for our egg ranch and the P2000 runs the same as with 8.1.
Created Date: August 04,2015
Created by: mls061
Our initial testing of Do-more Designer v1.4 and DirectSOFT v6.0 have shown no issues with Windows 10.
You still need to install the software "As Admininstrator " as with the earlier Windows OS's.
Created Date: August 14,2015
Created by: only1chip
Issue with CLICK USB driver (programming cable)
It may be something I'm doing wrong - but I get a "driver error " when the "Prolific USB-to-serial Comm Port " driver loads, when I connect the CLICK USB cable to my recently upgraded Windows 10 PC...
Windows only option seems to be "remove device "... Tried that, plugged cable in again - "Driver Error " again...
Went into device manager and had Windows check for a more recent version of the driver - and was told that I have the most recent version.
I 've got other (non Win10) machines - so it's not show stopper...
Any ideas?
Created Date: June 08,2016
Created by: genebond
For some reason, Windows 10 (Home) wants to substitute the 'Prolific ' driver on me every time I turn my back (arrrg!)
I have to go into Device Mangler and manually update the drive to the 'Koyo ' driver in order to use the cable.
I 've not figured out a way to tell Windows to leave well enough alone!
Anyone?
Created Date: June 08,2016
Created by: scott.lawrence
I 've not figured out a way to tell Windows to leave well enough alone!
Anyone?
uninstall W10, reinstall W7
Created Date: June 08,2016
Created by: andremholmes
This is what I do to avoid usb driver signature issues with Windows 8.1 &10
Select the Start button, then choose Settings.
Select Update & security> Recovery.
Under Advanced startup select Restart now.
After your PC restarts to the Choose an option screen, select Troubleshoot> Advanced options> Startup Settings> Restart.
After your PC restarts, select a startup setting by pressing the corresponding number(F7).
Created Date: August 01,2015
Created by: gringogreg
Have there been any issues yet with any AD software running on windows 10
DS6, DoMore designer, CMore micro, etc.