adccommunitymod (AutomationDirect) asked a question.
Created Date: December 14,2013
Created By: Ridgeline Mach
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
1. It would be nice if they added the features I'm accustomed to from using other Widows based software; Crtl-X for Cut, Cntl-C for Copy, and Cntl-V for paste. 2. While editing a program, and in haste, I may forget a connection (or some other syntax error) and just hit enter when the warning window pops up. Well, that defaults to, "delete the offending rungs. " The default should be correct the offending rungs. I 've had to re-write the code and that was frustrating. 3. When adding a branch, it seems it must be added in a certain order. In my brief time with the software (writing one program,) I had to add the vertical line first before adding the contacts below the main branch. Why cant there be a pencil tool (like the Click software) to add connections? Then order of what gets written when does not matter. 4. I'm wondering what is the benefit of the ONDTMR over the TMR? It just seems redundant that the ONDTMR operates a C register. Seems it would use more memory, plus one must remember which C register the ONDTMR controls rather than just remembering the timer number.
Created Date: December 14,2013
Created by: plcnut
In regards to number 1:
I use these all the time in DMD, where do they not work?
In regards to number 3:
You can use CTRL+arrow keys to draw wires, and SHFT+CTRL+arrow keys to delete wires. This way you quickly draw whatever you need and then type the syntax.
Just hoping to help ;)
Created Date: December 15,2013
Created by: LWgreys
DMD seemed to have an editing problem. I have already ran into them and alerted DMD developers. They plan on releasing a maintenance release to address these problems soon. Not sure when, but soon.
Created Date: December 17,2013
Created by: BobO
1. It would be nice if they added the features I'm accustomed to from using other Widows based software; Crtl-X for Cut, Cntl-C for Copy, and Cntl-V for paste.
Those keys should be supported everywhere the function is supported. Unfortunately those edit functions are rung level functions, not instruction level.
2. While editing a program, and in haste, I may forget a connection (or some other syntax error) and just hit enter when the warning window pops up. Well, that defaults to, "delete the offending rungs. " The default should be correct the offending rungs. I 've had to re-write the code and that was frustrating.
That's a good point.
3. When adding a branch, it seems it must be added in a certain order. In my brief time with the software (writing one program,) I had to add the vertical line first before adding the contacts below the main branch. Why cant there be a pencil tool (like the Click software) to add connections? Then order of what gets written when does not matter.
The order is irrelevant...but...growth of the matrix isn't. DmD's display is an array of matrices. You can only draw wires (use Ctrl+Arrows) within a matrix. Each rung number (or address) is associated with a matrix, so you can see the limits of the matrix you are editing within. My guess is that you were adding instructions to the next matrix, rather than expanding the one you meant to edit.
If you need to join two matrices, use Edit->Merge to join a rung up or down. That will take the contents of the two rungs and load them into a single matrix.
4. I'm wondering what is the benefit of the ONDTMR over the TMR? It just seems redundant that the ONDTMR operates a C register. Seems it would use more memory, plus one must remember which C register the ONDTMR controls rather than just remembering the timer number.
It's completely redundant, but for a purpose. Customers switching from other vendors ' products (AB, for instance) are accustomed to having On Delay and Off Delay timers. In an effort to meet customers half-way, we have provided touches like that where possible.
Created Date: December 17,2013
Created by: franji1
We fixed number 2 (default behavior will be to keep disconnected ladder instructions and let you go back and address them)
We added a new option to help new users in regards to #3. The default is to maintain an empty row in a rung while editing a rung. So as soon as you edit/add a contact, coil or box in a rung, an empty row is added at the bottom of THAT rung. This helps in the following ways:
1. The yellow bar that designates a modified rung shows up along all the rows in the margin of THAT rung, delineating its height with adjacent rungs (yellow bar will include the newly inserted row)
2. Makes it easier to add parallel contact branches or additional output boxes (the empty row is there already - no need to do Insert, Row, After Cursor)
If existing users (or new users) don't want this behavior, you can turn it off in the Ladder Options dialog.
This will be in our next maintenance release.
Created Date: December 24,2013
Created by: kewakl
In regards to number 1:
I use these all the time in DMD, where do they not work?
Copy/Paste single instruction?
Created Date: December 24,2013
Created by: BobO
Copy/Paste single instruction?
Hoping to add. Still not there, though.
Created Date: December 24,2013
Created by: plcnut
Copy/Paste single instruction?
No. I took it to mean copy/pasting whole rungs. Sorry.
Created Date: December 25,2013
Created by: Ridgeline Mach
Thank you all for the responses.
Yes, for number 1 I should have been specific and wrote whole rungs or a number of rungs. I made the mistake of writing code for a subroutine into the wrong subroutine. I wanted to just cut and paste the offending rungs and place them in the proper subroutine, and found the Do-More work around kind of cumbersome when accustomed to Windows native commands.
I find the response of the timer interesting. I write programs for the Click on our slower applications too, and it's just the pick of a radio button to change it from an on-delay to off-delay. I guess that's just not possible or native to the Do-More?
Created Date: December 26,2013
Created by: plcnut
Yes, for number 1 I should have been specific and wrote whole rungs or a number of rungs. I made the mistake of writing code for a subroutine into the wrong subroutine. I wanted to just cut and paste the offending rungs and place them in the proper subroutine, and found the Do-More work around kind of cumbersome when accustomed to Windows native commands.
Whole rung(s) can easily be done.
SHIFT + Up/Down Arrows to select the rungs, Then CTRL+C/X to Copy/Cut, Then CTRL+V to paste above your cursor.
Created Date: December 26,2013
Created by: franji1
Then CTRL+P to paste above your cursor. Ctrl+V does the paste, inserting the rung(s) within the code-block, above the current rung that has the colored block cursor (i.e. where input focus is located; a gray block cursor shows location, but does not designate input focus, i.e. where a key stroke such as a paste operation occurs; so you can have multiple gray block cursors but only 1 colored block cursor, the one that has input focus).