adccommunitymod (AutomationDirect) asked a question.
Cable for Do More Help
Created Date: January 30,2013
Created By: trimixdiver1
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
What is the cable I need for the DoMore to connect to an FA-ISOCON via the RJ12? Thanks
Created Date: January 30,2013
Created by: bcarlton
If you have ordered the FA-ISOCON the correct cable should come with it. Otherwise I believe it is the DV-1000CBL.
Created Date: January 30,2013
Created by: trimixdiver1
So if I made a cable:
CPU FA-ISOCON
Pin 1 0v Pin 1 0v
Pin 2 +5v Pin 5 +5v
Pin 3 RXD Pin 4 TXD
Pin 4 TXD Pin 3 RXD
Pin 5 RTS Pin 2 CTS
Pin 6 CTS Pin 6 GND
What about Pin 6?
Is this correct?
Thanks
Created Date: January 30,2013
Created by: bcarlton
Refer to the cable pinouts in the FA-ISOCON manual . It would be the same as connecting to a DL240, DL06, DL05 etc.
Created Date: January 30,2013
Created by: trimixdiver1
What is the cable I need for the DoMore to connect to an FA-ISOCON via the RJ12?
Thanks