adccommunitymod (AutomationDirect) asked a question.

Retentive Variables

Created Date: July 24,2019

Created By: kcress

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Seems my P2 program keeps the retentive values across power cycles but forgets them all across program updates. Without any switches flipped in Tools >Options >Program Transfer is this what's expected? Should I check both the Copy and Upload boxes to keep my retentive values across program updates?


  • adccommunitymod (AutomationDirect)

    Created Date: July 24,2019

    Created by: kcress

    Seems my P2 program keeps the retentive values across power cycles but forgets them all across program updates. Without any switches flipped in Tools>Options>Program Transfer is this what's expected?

    Should I check both the Copy and Upload boxes to keep my retentive values across program updates?

  • adccommunitymod (AutomationDirect)

    Created Date: July 24,2019

    Created by: ADC_CommTeam02

    Yes for stop mode transfers. Please refer to help topic P082 under Project Transfer Tab.

    Run time transfers do not effect retentive values.

  • adccommunitymod (AutomationDirect)

    Created Date: July 25,2019

    Created by: kcress

    Interesting, thanks for the info.. Makes sense.

    Thanks again P3K!

  • adccommunitymod (AutomationDirect)

    Created Date: July 25,2019

    Created by: JulesTop

    Yeah, It's unfortunate that those settings are not enabled by default as in an industrial environment, it's extremely risky.

    Imagine some sort of crisis and you get someone in the middle of the night to log into the PLC but they just installed Productivity Suite and didn't enable those settings... welp, they just wiped out all retentive tags... guess you can scrap that production run... and potentially a ton of parameters that dialed in the machine mechanics.

    Small things like this make a huge difference.

    I hope the development team takes note and changes the settings to be enabled by default.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 25,2019

    Created by: kewakl

    Yeah, It's unfortunate that those settings are not enabled by default as in an industrial environment, it's extremely risky.

    Imagine some sort of crisis and you get someone in the middle of the night to log into the PLC but they just installed Productivity Suite and didn't enable those settings... welp, they just wiped out all retentive tags... guess you can scrap that production run... and potentially a ton of parameters that dialed in the machine mechanics.

    Small things like this make a huge difference.

    I hope the development team takes note and changes the settings to be enabled by default.

    Or maybe this could be stored in the project on a per-project basis. Then it would not matter if Bubba just installed the suite the uploaded project would have the desired config.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 26,2019

    Created by: kcress

    Excellent points gentlemen! The project I'm working on has 4 measly rententives so I just re-entered them every time about 8 times until I could focus on the annoyance of the problem. I didn't think about a project with a couple of hundred retentives, a couple of them maybe arrived at by some long drawn-out calibration process.. All of them being pasted by an upload. That would be a catastrophe in some cases. Thanks for bringing that bigger picture up.

    I agree - they should default to save and upload.

    BTW I don't recall having this problem with all my CLICK projects. Could CLICK have this as the default?

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 26,2019

    Created by: kewakl

    In a click DS. DD, DH and DF default to retentive. Depending on sw ver, TXT may be retentive by default.

    Each register can be retenti v e or not.

    look in Tag Picker at the Retentive column.

  • adccommunitymod (AutomationDirect)

    Created Date: July 29,2019

    Created by: MikeN

    When doing a runtime transfer the retentive are not affected. When doing a stop mode transfer, by default doesnt it already ask you whether to keep the values or zero them out? Why go through the trouble of defaulting to always keep them when the choice comes up on its own and is just one button click? Also it is the first button in the row and is highlighted by default. So if you are just hitting enter a bunch it will save the retentive values.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 30,2019

    Created by: Todd Dice

    If I had one wish for P-suite (besides user defined data), it would be for it to store the values to all the registers in the offline project, just like RSLogix. This way when you do get the Bubba call, you can tell him from your copy of the offline project, what the value(s) are supposed to be for each register. :)

  • adccommunitymod (AutomationDirect)

    Created Date: August 05,2019

    Created by: kcress

    Hi kewakl;

    I see the default retentives in the CLICK. Includes a bunch of timers too.

    MikeN ;

    Good point. Just press The Right Button .

    Todd Dice;

    An excellent idea.

    My also P-Suite wish would be individual line comment formatting so I could change comment colors at will.

    Expand Post