adccommunitymod (AutomationDirect) asked a question.

P1 lost 'constant values' in code

Created Date: May 14,2019

Created By: kewakl

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

FW 1.2.7.37 SW 3.4.0.16 Constant (CODE) values in rungs are ALL ZERO This happened after one of the times that the software indicates that the P1 dropped out of RUN mode and then back into RUN mode during a RUN-TIME TRANSFER. I know when this happens because my HMI menu handler (snippet pictured) fails to work. Power cycle recovered. -- Glad that the machine was NOT in process at the time. The error log has three watchdog timeouts for today - all of which have happened during a runtime transfer. Normally, the scan time is about 1.2 mSec. 14MAY19 09:44:05 E03901 Watchdog TimeoutE:67 is the (last) error history entry Not every runtime transfer will have this WTD error. since power cycle Peak Scan Interval 48 Peak Logic Scan Time 19 Hardware config Max scan interval 500 mSec 600 bytes retentive { "data-align ": "none ", "data-size ": "full ", "data-attachmentid ":122698}


  • adccommunitymod (AutomationDirect)

    Created Date: May 14,2019

    Created by: kewakl

    FW 1.2.7.37

    SW 3.4.0.16

    Constant (CODE) values in rungs are ALL ZERO

    This happened after one of the times that the software indicates that the P1 dropped out of RUN mode and then back into RUN mode during a RUN-TIME TRANSFER.

    I know when this happens because my HMI menu handler (snippet pictured) fails to work. Power cycle recovered. -- Glad that the machine was NOT in process at the time.

    The error log has three watchdog timeouts for today - all of which have happened during a runtime transfer. Normally, the scan time is about 1.2 mSec.

    14MAY19 09:44:05 E03901 Watchdog TimeoutE:67 is the (last) error history entry

    Not every runtime transfer will have this WTD error.

    since power cycle

    Peak Scan Interval 48

    Peak Logic Scan Time 19

    Hardware config Max scan interval 500 mSec

    600 bytes retentive

    { "data-align ": "none ", "data-size ": "full ", "data-attachmentid ":122698}

    Expand Post