adccommunitymod (AutomationDirect) asked a question.

Productivity P1k rs-232 ASCII rfid

Created Date: March 12,2019

Created By: mfp101

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Hi Guys, I am trying to find a good way of authenticating users of my machines. Our I.T. department uses rfid readers to authenticate users of their applications and so I thought I would try reading the same id cards into my PAC. I purchased a rs232 rfid reader from RFIDeas (RDR-60W1AK5) which came with a db9 interface. I cut this and purchased a RJ12 keystone and straight through cable to connect to my P1k. This is the manual for the device: https://www.rfideas.com/files/downlo...CII_Manual.pdf I am able to write to the device with no issue (can change the LED and make beep) but am not getting anything if I try to read from it... My AIN instruction is always enabled but when I scan a card, nothing goes into the destination tag. I have tried this instruction with a variable number of characters with termination code 0x0d - no change. Any assistance would be much appreciated.


  • adccommunitymod (AutomationDirect)

    Created Date: March 12,2019

    Created by: mfp101

    Hi Guys,

    I am trying to find a good way of authenticating users of my machines. Our I.T. department uses rfid readers to authenticate users of their applications and so I thought I would try reading the same id cards into my PAC.

    I purchased a rs232 rfid reader from RFIDeas (RDR-60W1AK5) which came with a db9 interface. I cut this and purchased a RJ12 keystone and straight through cable to connect to my P1k.

    This is the manual for the device:

    https://www.rfideas.com/files/downlo...CII_Manual.pdf

    I am able to write to the device with no issue (can change the LED and make beep) but am not getting anything if I try to read from it...

    My AIN instruction is always enabled but when I scan a card, nothing goes into the destination tag. I have tried this instruction with a variable number of characters with termination code 0x0d - no change.

    Any assistance would be much appreciated.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 12,2019

    Created by: OldControl

    Questions

    1 have you setup the rfid card with the rfid software to the correct card total chars parsing rules and seen the card chars read into your computer

    2 why use an aout to read as a valid card swept by reader can send the string

    stick with fixed length ain for now at least you will see something even if wrong baud rate etc

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 12,2019

    Created by: IMNCTRL

    This is a RS-232 network. It is point to point and there can only be one master device and one slave device. The plc should be the master and use an AOUT command to request the id from the device. ( Looks like one of the rfid:qid commands) After the AOUT is complete the AIN should be enabled to look for the response from the slave device. (RFID reader) I do not see anywhere in the manual that they send a termination code or that you can specify one, but they give detailed data on what is in the string so you will have to use string function instructions to extract the data you wish to use.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: March 25,2019

    Created by: lessmorethan

    On a new serial device, I always use the pc and realterm first to verify my custom ascii before committing to the plc.

  • adccommunitymod (AutomationDirect)

    Created Date: March 25,2019

    Created by: mfp101

    Thanks guys, I figured it out the devices transmit signal was not making good contact.

  • adccommunitymod (AutomationDirect)

    Created Date: October 29,2019

    Created by: Bfeddeck

    Can you post you code? I'm doing something similar and this looks like a good starting point.