adccommunitymod (AutomationDirect) asked a question.
Created Date: June 28,2018
Created By: kewakl
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
In some future rev, can we get a nagging issue fixed? I understand that there are many and several nagging issues, but this one just wasted my time again. If the Set CPU Time/Date dialog is set to the smallest horizontal size (which SHOULD BE THE DEFAULT SIZE) the and do not show. The button is to the far right (why should it ever appear there?) which would imply that there are no more options to be had. This is present in ver 1.9.2.0 and 3.2.2.4. Sometimes I feel like an unpaid alpha tester.
Created Date: June 28,2018
Created by: kewakl
In some future rev, can we get a nagging issue fixed? I understand that there are many and several nagging issues, but this one just wasted my time again.
If the Set CPU Time/Date dialog is set to the smallest horizontal size (which SHOULD BE THE DEFAULT SIZE) the and do not show. The button is to the far right (why should it ever appear there?) which would imply that there are no more options to be had.
This is present in ver 1.9.2.0 and 3.2.2.4. Sometimes I feel like an unpaid alpha tester.
Created Date: June 28,2018
Created by: ADC_CommTeam01
What is your screen resolution and your screen magnification set to?
Created Date: June 28,2018
Created by: kewakl
Default for monitor and 100%- Purely default and default. Should that matter?
I have seen better-behaved software have NO issue with screen resolution.
The software for PAC and SOLO seem to be the worst offenders in this area. --
btw, they are java-based, right?
The 'InstallAnywhere ' dialog tells me that.MS SpyXX reporting the SunAw t Frame confirms it.
Created Date: June 28,2018
Created by: Ridgeline Mach
I do not have this issue, and I am using a 17 " Toshiba Satellite L55-B5294 Windows 7 Pro laptop.
kewakl, can you post a screenshot?
Created Date: June 29,2018
Created by: ADC_CommTeam01
kewakl
we had a QA guy trying to duplicate and could not make the window small enough to hide the buttons. I also tried with no success. We were TRYING to get more info.
Created Date: June 29,2018
Created by: kewakl
short vid clip from home using camtasia camstudio recorder
looks the same at the shop. I'll try all the revs that I have installed.
Created Date: June 29,2018
Created by: kewakl
kewakl
We were TRYING to get more info.
:o
Understood. Thanks.
Created Date: June 29,2018
Created by: kewakl
I do not have this issue, and I am using a 17 " Toshiba Satellite L55-B5294 Windows 7 Pro laptop.
kewakl, can you post a screenshot?
thanks. Did just a bit better than screenshot.
Created Date: June 29,2018
Created by: kewakl
and on laptop
both win7 pro sp1
homepc has MSI RX 480 8GB.
This laptop is a crummy HP zbook with intel HD and invidia quadro M1000M video 1920X1080
This clip is from V1.7.1.1
Created Date: June 29,2018
Created by: ADC_CommTeam01
Can you:
1) Start a new instance of the GUI with no other instances open. ( Preferably 3.2.2.4)
2) Make this happen.
3) Send the log file from the following location on your pc C:\ProgramData\AutomationDirect\Productivity Suite 3.2.2.4 ( or whatever version you reproduce it on.)