adccommunitymod (AutomationDirect) asked a question.

P2-550 To an SMC EX260-SEN1 Valve Adapter

Created Date: April 18,2018

Created By: larryhts

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am having trouble with an EtherNet/IP client to communicate with a SMC EX260-SEN1 ValveBank adapter. I get the TCP connected and the adapter name vendor code but an error 0x128. I have tried these on AB processors and this is the first P2-550 for us. Any insight would help. Thanks


  • adccommunitymod (AutomationDirect)

    Created Date: April 18,2018

    Created by: larryhts

    I am having trouble with an EtherNet/IP client to communicate with a SMC EX260-SEN1 ValveBank adapter. I get the TCP connected and the adapter name vendor code but an error 0x128.

    I have tried these on AB processors and this is the first P2-550 for us. Any insight would help. Thanks

  • adccommunitymod (AutomationDirect)

    Created Date: April 18,2018

    Created by: ADC_CommTeam01

    { "data-align ": "none ", "data-size ": "medium ", "data-attachmentid ":112627} Topic P260 of the help file:

    { "alt ": "Click image for larger version Name:\teip.JPG Views:\t1 Size:\t101.5 KB ID:\t112625 ", "data-align ": "none ", "data-attachmentid ": "112625 ", "data-size ": "full ", "title ": "eip.JPG "}

  • adccommunitymod (AutomationDirect)

    Created Date: April 18,2018

    Created by: larryhts

    I have it working now Here are the settings::

    8 bit int, Swap Byte on, and on the output Include Status Header

    input instance = 100

    Integer 8 bit

    Elements 2

    Output Instance = 150 and Include Status Header on

    Integer 8 Bit

    Elements 4

    Config

    Instance = 105

    Integer 8 Bit

    Elements 0

    Thanks Larry

    Expand Post