adccommunitymod (AutomationDirect) asked a question.

P2K Not Saving Properly

Created Date: February 17,2018

Created By: robertkeenan

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I have a PLC which is not saving the project in the normal way. Project File Status = Not Saved CPU Project Status = Out Of Date Transfer the project to the PLC and Project File Status = Not Saved CPU Project Status = Up to Date Now save the file to the PC and Project File Status = Saved CPU Project Status = Out Of Date Transfer the project to the PLC and Project File Status = Not Saved CPU Project Status = Up to Date I can not get the two of them to be happy with the saved project, either one is out of date or the other is not saved. If I close the project and then reconnect it will say that there is Project Differences, but I know that they are the same. The only error showing on the error history is E04204 DL Buffer > 50% Full and memory usage is 6%. n111436


  • adccommunitymod (AutomationDirect)

    Created Date: February 17,2018

    Created by: robertkeenan

    I have a PLC which is not saving the project in the normal way.

    Project File Status = Not Saved

    CPU Project Status = Out Of Date

    Transfer the project to the PLC and

    Project File Status = Not Saved

    CPU Project Status = Up to Date

    Now save the file to the PC and

    Project File Status = Saved

    CPU Project Status = Out Of Date

    Transfer the project to the PLC and

    Project File Status = Not Saved

    CPU Project Status = Up to Date

    I can not get the two of them to be happy with the saved project, either one is out of date or the other is not saved. If I close the project and then reconnect it will say that there is Project Differences, but I know that they are the same. The only error showing on the error history is E04204 DL Buffer> 50% Full and memory usage is 6%. n111436

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 19,2018

    Created by: ADC_CommTeam01

    In your task named "Loading Bay Temperatures " you have a subrung "3.1 " that has an END, but is not attached to rung 3. Delete this subrung and it should save.

    { "data-align ": "none ", "data-size ": "full ", "title ": "Rung.JPG ", "data-attachmentid ":111458}

  • adccommunitymod (AutomationDirect)

    Created Date: February 19,2018

    Created by: kewakl

    In your task named "Loading Bay Temperatures " you have a subrung "3.1 " that has an END, but is not attached to rung 3. Delete this subrung and it should save.

    { "alt ": "Click image for larger version Name:\tRung.JPG Views:\t1 Size:\t36.4 KB ID:\t111458 ", "data-align ": "none ", "data-attachmentid ": "111458 ", "data-size ": "full ", "title ": "Rung.JPG "}

    Maybe an update so the software could flag that.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: February 20,2018

    Created by: Brandon_

    Why isn't the compiler giving an error on that? More so, why is that an issue at all?

    Interestingly, I ran into the very same problem today. Save program> Program Up to date. Transfer program (runtime)> CPU up to date, but then immediately the program would not be up to day. Re-save the program> program up to date, immediately CPU becomes not up to date.

    Closed everything out, rebooted laptop (it had been up for quite a few days without a reboot), issue disappeared.

    Expand Post