adccommunitymod (AutomationDirect) asked a question.

P1K Math Issue

Created Date: January 18,2018

Created By: pbw

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

So I bought a P1K to check it out. Did a little coding to get a feel for the machine and ran into a math issue. Why does this formula not Work? It compiles okay but returns "NaN ". { "alt ": "Click image for larger version Name:\tProblem.PNG Views:\t3 Size:\t3.7 KB ID:\t110450 ", "data-align ": "none ", "data-attachmentid ": "110450 ", "data-size ": "full "} I tore the formula apart and it appears its the back end that was causing grief so I dropped that into a different Math box and it works { "data-align ": "none ", "data-attachmentid ": "110449 ", "data-size ": "full "} I got the same formula running on a Do-More Cpu without issue what gives:confused:


  • adccommunitymod (AutomationDirect)

    Created Date: January 18,2018

    Created by: pbw

    So I bought a P1K to check it out. Did a little coding to get a feel for the machine and ran into a math issue.

    Why does this formula not Work? It compiles okay but returns "NaN ".

    { "alt ": "Click image for larger version Name:\tProblem.PNG Views:\t3 Size:\t3.7 KB ID:\t110450 ", "data-align ": "none ", "data-attachmentid ": "110450 ", "data-size ": "full "}

    I tore the formula apart and it appears its the back end that was causing grief so I dropped that into a different Math box and it works

    { "data-align ": "none ", "data-attachmentid ": "110449 ", "data-size ": "full "}

    I got the same formula running on a Do-More Cpu without issue what gives:confused:

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 18,2018

    Created by: pbw

    My bad. Please disregard

    I forgot to pre-compute "Temp File " and "RH File "