adccommunitymod (AutomationDirect) asked a question.

Productivity 1000 programming help

Created Date: December 06,2017

Created By: DerekKrehling

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I'm attempting my first shot at PLC programming in about 5 years with a Productivity 1000 PLC. I am retrofitting an older boring machine that is pretty simple. I think i have the majority of it figured out - but have a few issues I'm stuck on. On the first line there is an output "hold down clamp solenoid " - I cannot get this output to "latch. " The output will only engage when I hold the start button. I can also not get the timers to start. I'm assuming that there's something simple I'm missing but I can't seem to figure it out. A brief synopsis of the machine function - It is a three head boring machine, with air cylinders that move the motor assemblies to do the actual drilling. You can select any 1, 2 or 3 motors to run at the same time by flipping selector switch on the operator panel. When you press the start button the hold down cylinder will come on along with the selected motors. There is a delay to allow the motors to come up to speed, then the drilling cylinders activate. When it gets to the end of the stroke it hits a limit switch which will turn off the drilling cylinders. There will be a delay to allow the cylinders to retract, then the motors and hold down cylinder will turn off. I would appreciate any help I can get on this. The photo shows the programming for motor 1 - the rest of the program repeats for motors 2 and 3. { "data-align ": "none ", "data-size ": "full ", "data-attachmentid ":109585}


  • adccommunitymod (AutomationDirect)

    Created Date: December 06,2017

    Created by: DerekKrehling

    I'm attempting my first shot at PLC programming in about 5 years with a Productivity 1000 PLC. I am retrofitting an older boring machine that is pretty simple. I think i have the majority of it figured out - but have a few issues I'm stuck on. On the first line there is an output "hold down clamp solenoid " - I cannot get this output to "latch. " The output will only engage when I hold the start button. I can also not get the timers to start. I'm assuming that there's something simple I'm missing but I can't seem to figure it out.

    A brief synopsis of the machine function - It is a three head boring machine, with air cylinders that move the motor assemblies to do the actual drilling. You can select any 1, 2 or 3 motors to run at the same time by flipping selector switch on the operator panel. When you press the start button the hold down cylinder will come on along with the selected motors. There is a delay to allow the motors to come up to speed, then the drilling cylinders activate. When it gets to the end of the stroke it hits a limit switch which will turn off the drilling cylinders. There will be a delay to allow the cylinders to retract, then the motors and hold down cylinder will turn off.

    I would appreciate any help I can get on this. The photo shows the programming for motor 1 - the rest of the program repeats for motors 2 and 3.

    { "data-align ": "none ", "data-size ": "full ", "data-attachmentid ":109585}

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: December 06,2017

    Created by: RogerR

    Possible that the program has been edited and not downloaded to the plc.

    Line 1 contains the start button and the hold in contact in parallel that should keep it turned on.

    This line 1 shows an edit.

  • adccommunitymod (AutomationDirect)

    Created Date: December 06,2017

    Created by: DerekKrehling

    I did reload the program after this picture was taken - I just added the retract timers back in after making edits to try to troubleshoot

  • adccommunitymod (AutomationDirect)

    Created Date: December 06,2017

    Created by: ADC_CommTeam02

    Did you assign DO-0.1.1.1 to another output instruction? You could have another rung that is forcing off that output thus overwriting your first rung. If you need to use an output to be used on multiple rungs you have to use an OR OUT for the coil.

    { "data-align ": "none ", "data-attachmentid ": "109590 ", "data-size ": "large "}

  • adccommunitymod (AutomationDirect)

    Created Date: December 06,2017

    Created by: Mike Nash

    I don't have the PAC software loaded, but if the Retract Timers are in milliseconds, then a 0.15 second on time is all you can expect.

  • adccommunitymod (AutomationDirect)

    Created Date: December 06,2017

    Created by: DerekKrehling

    Timers are in centiseconds (.01). Im not using the output anywhere else.

  • adccommunitymod (AutomationDirect)

    Created Date: December 07,2017

    Created by: techme

    Is the plc in run? In this pic it is in Stop.

  • adccommunitymod (AutomationDirect)

    Created Date: December 07,2017

    Created by: techme

    1) In the picture the plc is in Stop mode. I know you said you see the output come on, but wanted to make sure you had in in Run.

    2) on rung #7 is that a reset? If so go to rung #8 and insert a rung above rung #8 and put an end statement and then test logic.

    I entered this exact same logic here and it works as expected.

    { "data-align ": "none ", "data-size ": "large ", "data-attachmentid ":109599}

    Expand Post