adccommunitymod (AutomationDirect) asked a question.
Productivity Version 2.4.0 (16) Force Bit From Data View
Created Date: September 28,2017
Created By: IBS Guy
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Using Forceable Tags Tab: After unchecking some of the tag FORCE boxes, they would recheck themselves when I checked other tag Force Boxes. The only way to clear the slate was to uncheck everything else first then uncheck the troublemakers and close the data view. Outta sight, outta mind.
Created Date: September 28,2017
Created by: IBS Guy
Using Forceable Tags Tab: After unchecking some of the tag FORCE boxes, they would recheck themselves when I checked other tag Force Boxes. The only way to clear the slate was to uncheck everything else first then uncheck the troublemakers and close the data view. Outta sight, outta mind.
Created Date: September 28,2017
Created by: kewakl
{ "alt ": "Click image for larger version Name:\tforces.png Views:\t1 Size:\t13.9 KB ID:\t108238 ", "data-align ": "none ", "data-attachmentid ": "108238 ", "data-size ": "full "}
I can somewhat duplicate this in 2.4.4.1 - If I have duplicate forceable tags in the same dataview, I have to be careful when checking/unchecking that force checkbox.
Also, the force status does not propagate to all duplicate tags, as does the EDIT checkbox value.
EDIT: P3-550 FW 1.1.15.104