adccommunitymod (AutomationDirect) asked a question.

Add mixed P3000+P2000 compatibility

Created Date: July 12,2017

Created By: MikeN

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

Right now in the Productivity software you can drag 'n drop different chassis into remote units and select the remote slave you are using in the chassis. However you cannot be using a P3000, and add in a remote P2000 this way. You can only select other systems of the same type you have as your main base chassis. Since the platforms are extremely similar, support should be added so that you can mix the two models in a system and have remote units be whatever model of Productivity you want. { "alt ": "Click image for larger version Name:\tdragndrop.png Views:\t1 Size:\t33.2 KB ID:\t107022 ", "data-align ": "none ", "data-attachmentid ": "107022 ", "data-size ": "full "} Also, could you add a 15 slot base for the P3000's? Sure it would take up a lot of width, but it would be nice to be able to have more high speed output capabilities on the 3000 platform


  • adccommunitymod (AutomationDirect)

    Created Date: July 12,2017

    Created by: MikeN

    Right now in the Productivity software you can drag 'n drop different chassis into remote units and select the remote slave you are using in the chassis. However you cannot be using a P3000, and add in a remote P2000 this way. You can only select other systems of the same type you have as your main base chassis. Since the platforms are extremely similar, support should be added so that you can mix the two models in a system and have remote units be whatever model of Productivity you want.

    { "alt ": "Click image for larger version Name:\tdragndrop.png Views:\t1 Size:\t33.2 KB ID:\t107022 ", "data-align ": "none ", "data-attachmentid ": "107022 ", "data-size ": "full "}

    Also, could you add a 15 slot base for the P3000's? Sure it would take up a lot of width, but it would be nice to be able to have more high speed output capabilities on the 3000 platform

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 12,2017

    Created by: kewakl

    Right now in the Productivity software you can drag 'n drop different chassis into remote units and select the remote slave you are using in the chassis. However you cannot be using a P3000, and add in a remote P2000 this way. You can only select other systems of the same type you have as your main base chassis. Since the platforms are extremely similar, support should be added so that you can mix the two models in a system and have remote units be whatever model of Productivity you want.

    { "alt ": "Click image for larger version Name:\tdragndrop.png Views:\t1 Size:\t33.2 KB ID:\t107022 ", "data-align ": "none ", "data-attachmentid ": "107022 ", "data-size ": "full "}

    Also, could you add a 15 slot base for the P3000's? Sure it would take up a lot of width, but it would be nice to be able to have more high speed output capabilities on the 3000 platform

    I would be like to again have the ability to post images/files to this forum.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: July 18,2017

    Created by: bdehner

    Thanks for the post. I have made the Product Engineers aware of your request.