adccommunitymod (AutomationDirect) asked a question.
User function or similar in Productivity or Do-More
Created Date: April 27,2016
Created By: g.mccormick
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I believe that AB calls these "AOI " for "add-on-instructions ". In Codesys, they are functions. Is there the ability to created user defined functions/blocks/AOI that can be called in either Do-More or Productivity series?
Created Date: April 27,2016
Created by: g.mccormick
I believe that AB calls these "AOI " for "add-on-instructions ". In Codesys, they are functions.
Is there the ability to created user defined functions/blocks/AOI that can be called in either Do-More or Productivity series?
Created Date: April 27,2016
Created by: scott.lawrence
Do-More has structures, but I 've never used them to try to recreate an AOI
Created Date: April 27,2016
Created by: ADC_CommTeam02
Currently this is not available for the P Series product line. It is on our roadmap, however no time frame on a release.
Created Date: April 27,2016
Created by: g.mccormick
So would you suggest make a "function " of a subprocedure. Then copying/renaming subprocedure for each "function-call " needed?
Created Date: April 27,2016
Created by: franji1
Do-more is looking to implement a Subroutine CALL, where input parameters are passed-in and output parameters are returned via a "copy " mechanism, but the subroutine CALL literally jumps to that code-block, and executes until it hits a RETTURN, then returns back to the CALL in the original code-block. Currently, we can nest up to 80+ subroutine CALLs (A calls B which calls C which calls D, etc.). It's not quite USER BOXES (something else we also want to implement), but it's close.