adccommunitymod (AutomationDirect) asked a question.
P2000 task
Created Date: November 27,2015
Created By: christine
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
Hello! as a new user, am very sure that some of you ever had this problem. Im tring hard to be able to disable a part of my ladder(outputs ' without all the rest. So I try to but my outs in a 'Call Task 'But it appears that when the task is not Call the outputs are still on ??? Do I have to disable each rung with a NO CaLL contact Confused With AB i use a MRC coil is there something close p2-550 HELP Christine
Created Date: November 28,2015
Created by: Ridgeline Mach
Not sure, but the MCR command you 're asking about should NEVER be used as a safety to prevent output operation. The only safe MCR, is a Master Control Relay that is hard wired to disable power to your outputs.
What we do, in addition to a hard wired MCR, is have an input on the PLC monitor whether the MCR is energized, or not, through one of the normally open contacts of the MCR.
Created Date: November 30,2015
Created by: OkiePC
If you stop calling a task, the associated logic will no longer run and therefore the bits in the "coil " instructions will no longer alter the values of their bits.
In other words, the outputs will be left in the last state commanded the last time the task was called.
I am not a fan of MCR instructions. I would rather add a single "contact " or XIC instruction to every rung and have them all execute all the time. To disable those outputs, I can turn off that bit. I could understand using MCR type of programming only if you are out of program memory.
I am also an opponent of conditional subroutines in most cases. They have a place for certain types of math, but for normal control situations, I believe in running all the code all the time.
Using conditional routines to controls bits and especially real world outputs can lead to confusion and a convoluted program in the end.
Created Date: November 30,2015
Created by: Ridgeline Mach
If you stop calling a task, the associated logic will no longer run and therefore the bits in the "coil " instructions will no longer alter the values of their bits.
In other words, the outputs will be left in the last state commanded the last time the task was called.
I am not a fan of MCR instructions. I would rather add a single "contact " or XIC instruction to every rung and have them all execute all the time. To disable those outputs, I can turn off that bit. I could understand using MCR type of programming only if you are out of program memory.
I am also an opponent of conditional subroutines in most cases. They have a place for certain types of math, but for normal control situations, I believe in running all the code all the time.
Using conditional routines to controls bits and especially real world outputs can lead to confusion and a convoluted program in the end.
If I had been more complete in my response, I would have said that this is exactly what the input tied to my MCR does. It gives me dual redundancy of stopping a circuit.
Created Date: December 01,2015
Created by: Adisharr
I'm kind of in the same school of thought as Okie. All my code runs all the time unless it's so scan intensive that it interferes with something else. Doing that, you don't run into issues like described. I still split the code up into subroutines but each one is executed in order every scan cycle as if it were all one continuous block of code.
Created Date: December 01,2015
Created by: kewakl
If you stop calling a task, the associated logic will no longer run and therefore the bits in the "coil " instructions will no longer alter the values of their bits.
I am also an opponent of conditional subroutines in most cases. They have a place for certain types of math, but for normal control situations, I believe in running all the code all the time.
Using conditional routines to controls bits and especially real world outputs can lead to confusion and a convoluted program in the end.
And, as I have found (at least in earlier versions of P 3 K)
DO NOT PUT COMMS INSTRUCTIONS IN CALLED TASKS!
Created Date: November 27,2015
Created by: christine
Hello! as a new user, am very sure that some of you ever had this problem.
Im tring hard to be able to disable a part of my ladder(outputs ' without all the rest.
So
I try to but my outs in a 'Call Task 'But it appears that when the task is not Call
the outputs are still on ???
Do I have to disable each rung with a NO CaLL contact
Confused
With AB i use a MRC coil is there something close p2-550
HELP
Christine