adccommunitymod (AutomationDirect) asked a question.
P2000 Ascii to Integer
Created Date: October 12,2015
Created By: befraim
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
A Keyence SR-750 barcode reader is sending ASCII numbers via Ethernet/IP to P2000 CPU. How do I convert the ASCII info to integer?
Created Date: October 12,2015
Created by: ADC_CommTeam01
Use the CPC instruction to copy string to integer array.
Created Date: October 12,2015
Created by: bcarlton
It is possible that befraim is asking if an instruction similar to STR2INT in the Do-more is available.
Created Date: October 13,2015
Created by: befraim
Your correct Bernie. I was looking at the STR2INT instruction in D0-More and thinking it was what I need. The info comes into the P2000 CPU via Ethernet/IP and is placed into an array. I was looking for a way to change from the ASCII format to integer. I have been investigating the suggested CPC instruction and how to use it.
Created Date: October 13,2015
Created by: befraim
Here is the solution I ended up with. ASCII data comes onto the CPU and is stored in an array. COPY ARRAY instruction moves data I need into a second array. COPY CHARACTER instruction converts and stores data as a string. UNPACK STRING instruction converts and stores data as an integer. Let me know if there is a simpler or more elegant method to do this. Thanks for your help!
Created Date: October 12,2015
Created by: befraim
A Keyence SR-750 barcode reader is sending ASCII numbers via Ethernet/IP to P2000 CPU. How do I convert the ASCII info to integer?
Not really an answer, more of a bump and a question regarding the Ethernet/ip settings. We are tryiong to get the data from a Keyence SR-2000 reader and so far have been unable to get the string in anyway that we can use it/see it. Do you know what settings you used for the communications to the SR-730 reader?
This post was from back in 2015 and i don't any of these guys are still around.
I know i tested a keyence barcode scanner with a productivity 1000 like 5 years ago and was able to get it to work but i do not know if i still have the program. That project ended up going with a IFM barcode scanner because it was significantly cheaper for similar performance.
Thanks for the response. I kind of figure it was a long shot, but thought someone else might have figured something out.
we did actually manage to get the results from the reader, with a lot of trial and error. Once I get a cleaner version of the program I will try to post some screen shots of the settings that worked.
Thanks again, much appreciated.