adccommunitymod (AutomationDirect) asked a question.
Created Date: August 12,2015
Created By: KHILL
**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****
I am not sure if this has already been suggested, but during monitoring mode, it would be nice to see timer status on coil instructions with timers, such as Debounce, Flasher, and Timed Coils. It helps on debugging when you are waiting on coils with long durations. Also, it would be nice to be able to associate a tag with the timers, so that you can globally change many Coil timers at once. Sometimes I will have to use Timers or Simple Timers to get this option, but would rather stick with the simplicity that timed coils offer. Cheers!
Created Date: August 12,2015
Created by: ADC_CommTeam02
Thanks for the feed back. I have sent your suggestions over to our development team for evaluation. Keep the suggestions coming!
Created Date: August 12,2015
Created by: KHILL
I am not sure if this has already been suggested, but during monitoring mode, it would be nice to see timer status on coil instructions with timers, such as Debounce, Flasher, and Timed Coils. It helps on debugging when you are waiting on coils with long durations.
Also, it would be nice to be able to associate a tag with the timers, so that you can globally change many Coil timers at once. Sometimes I will have to use Timers or Simple Timers to get this option, but would rather stick with the simplicity that timed coils offer.
Cheers!