adccommunitymod (AutomationDirect) asked a question.

C-more and Email Addresses

Created Date: December 30,2019

Created By: djedesign1

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I find the Text Entry object lacking in some printable symbols that may be used for Email addresses. Both the Do-more/BRX/etc and the Productivity allow Strings to be used for a destination Email Addresses. It should be easy to change these through a C-More such as when a Plant Manager, Etc., changes but some symbols are missing. From Wikipedia: The local-part of the email address may use any of these ASCII characters: uppercase and lowercase Latin letters A to Z and a to z; digits 0 to 9; printable characters !#$% & '*+-/=?^_`{|}~; dot ., provided that it is not the first or last character unless quoted, and provided also that it does not appear consecutively unless quoted (e.g. John..Doe@example.com is not allowed but "John..Doe "@example.com is allowed); The is more, but I think this gives the minimum. Currently we can only enter dot, underline, and dash. Adding all the legal symbols would be helpful


  • adccommunitymod (AutomationDirect)

    Created Date: December 30,2019

    Created by: djedesign1

    I find the Text Entry object lacking in some printable symbols that may be used for Email addresses. Both the Do-more/BRX/etc and the Productivity allow Strings to be used for a destination Email Addresses. It should be easy to change these through a C-More such as when a Plant Manager, Etc., changes but some symbols are missing.

    From Wikipedia:

    The local-part of the email address may use any of these ASCII characters:

    uppercase and lowercase Latin letters A to Z and a to z;

    digits 0 to 9;

    printable characters !#$%& '*+-/=?^_`{|}~;

    dot ., provided that it is not the first or last character unless quoted, and provided also that it does not appear consecutively unless quoted (e.g. John..Doe@example.com is not allowed but "John..Doe "@example.com is allowed);

    The is more, but I think this gives the minimum. Currently we can only enter dot, underline, and dash.

    Adding all the legal symbols would be helpful

    Expand Post