adccommunitymod (AutomationDirect) asked a question.

EA9 Event Message Box

Created Date: January 24,2019

Created By: Bergie3941

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

I am wondering if anybody knows how to get a message box in an Event to go away automatically after a set amount of time, instead of requiring the operator to press OK? I have a start delay during which I want a message displayed, but then want it to go away when the time has run out. Currently the message box is set to show when the .TT bit is true.


  • adccommunitymod (AutomationDirect)

    Created Date: January 24,2019

    Created by: Bergie3941

    I am wondering if anybody knows how to get a message box in an Event to go away automatically after a set amount of time, instead of requiring the operator to press OK? I have a start delay during which I want a message displayed, but then want it to go away when the time has run out. Currently the message box is set to show when the .TT bit is true.

  • adccommunitymod (AutomationDirect)

    Created Date: January 25,2019

    Created by: Bergie3941

    Thanks for the reply, Tom@Pton. However, this doesn't seem to work for me. I have a message box and a sound set to go on when the .ACC is between a certain range, as suggested. The sound stops when outside of the range, but the message box stays on the screen until the OK button is pressed. I ended up just using a static text object and set it's visibility based on the .DN tag, seems to work fine.

    Expand Post