adccommunitymod (AutomationDirect) asked a question.

C-more ea9 request

Created Date: December 28,2018

Created By: z28z34man

**** This post has been imported from our legacy forum. Information in this post may be outdated and links contained in the post may no longer work.****

It would be awesome if there was a reduced feature 12 " touch screen available. There is the less expensive wide screen 10 " then it jumps to the reduced feature 15 ". I have a project that the 15 " is a bit big but the extra room on a 12 " would be nice but I have no need for the extra features on the full feature version. At your prices it not really a huge deal but just trying to get the most bang for the buck.


  • adccommunitymod (AutomationDirect)

    Created Date: December 28,2018

    Created by: z28z34man

    It would be awesome if there was a reduced feature 12 " touch screen available. There is the less expensive wide screen 10 " then it jumps to the reduced feature 15 ". I have a project that the 15 " is a bit big but the extra room on a 12 " would be nice but I have no need for the extra features on the full feature version.

    At your prices it not really a huge deal but just trying to get the most bang for the buck.

    Expand Post
  • adccommunitymod (AutomationDirect)

    Created Date: January 03,2019

    Created by: bdehner

    Thanks for the post. The Product Manager has been made aware of your request and will take it into consideration. Please let us know if there are any other needs you may have. Thanks again.